2017-08-29 1:02 PM
Hello everyone I am trying to interface acceleration sensor Adxl345 to stm32f302 through I2C using the HAL Library. Actually I am learning the programming , does any one help me how to get the data from sensor. I wrote this code , it does not work it.
void adxl345_data(void)
{
uint8_t data[2]; int x ; int data_1; char buff[100]; HAL_I2C_Mem_Read(&hi2c3, 0x53<<1, 0x32, I2C_MEMADD_SIZE_8BIT, (uint8_t*)data, 2, 1000); x = ( data[1]<<8) |data[0];}
could you give me idea where is mistake ?
2017-08-29 1:46 PM
Hello!
This is the right funtion to read the ADXL345
You use the second 0x53 address, make sure that SDO/ALT ADDRESS pin (Pin 12) is grounded. else use the 0x1D address.
I2C_MEMADD_SIZE_8BIT must be 1.
But this isn't the correct way to read the X_data.
Needs some initialization first .
Try first to read the DEVID register (address 0x00 , one byte) to check the functionality of your code.
Then initialise the chip (at least the power control register 0x2d )
Regards.
vf
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.