2013-11-01 12:55 AM
When i use the command
GPIO_PinAFConfig(GPIOB, GPIO_Pin_14 ,GPIO_AF_SPI2);the controller goes to a hardware fault.my init function is void SPI_FLASH_Init(void){ SPI_InitTypeDef SPI_InitStructure; GPIO_InitTypeDef GPIO_InitStructure; /* Enable SPI2, GPIOA and GPIOBclocks */ RCC_APB1PeriphClockCmd(RCC_APB1Periph_SPI2 , ENABLE); RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOB, ENABLE); /* Configure SPI2 pins: SCK, MISO and MOSI */ GPIO_PinAFConfig(GPIOB, GPIO_Pin_13 ,GPIO_AF_SPI2); GPIO_PinAFConfig(GPIOB, GPIO_Pin_14 ,GPIO_AF_SPI2); GPIO_PinAFConfig(GPIOB, GPIO_Pin_15 ,GPIO_AF_SPI2); /* Configure PB.2 as Output push-pull, used as Flash Chip select */ GPIO_InitStructure.GPIO_Pin = GPIO_Pin_12; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_OUT; GPIO_InitStructure.GPIO_OType = GPIO_OType_PP; GPIO_Init(GPIOB, &GPIO_InitStructure); GPIO_InitStructure.GPIO_Pin = GPIO_Pin_13 | GPIO_Pin_14 | GPIO_Pin_15; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF; GPIO_InitStructure.GPIO_OType = GPIO_OType_PP; GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL; GPIO_Init(GPIOB, &GPIO_InitStructure); /* Deselect the FLASH: Chip Select high */ SPI_FLASH_CS_HIGH(); /* SPI2 configuration */ SPI_InitStructure.SPI_Direction = SPI_Direction_2Lines_FullDuplex; SPI_InitStructure.SPI_Mode = SPI_Mode_Master; SPI_InitStructure.SPI_DataSize = SPI_DataSize_8b; SPI_InitStructure.SPI_CPOL = SPI_CPOL_High; SPI_InitStructure.SPI_CPHA = SPI_CPHA_2Edge; SPI_InitStructure.SPI_NSS = SPI_NSS_Soft; SPI_InitStructure.SPI_BaudRatePrescaler = SPI_BaudRatePrescaler_4; SPI_InitStructure.SPI_FirstBit = SPI_FirstBit_MSB; SPI_InitStructure.SPI_CRCPolynomial = 7; SPI_Init(SPI2, &SPI_InitStructure); /* Enable SPI2 */ SPI_Cmd(SPI2, ENABLE); }2013-11-01 4:15 AM
GPIO_PinAFConfig(GPIOB, GPIO_Pin_14 ,GPIO_AF_SPI2);
GPIO_PinSource14GPIO_PinAFConfig wants an index (PinSource) not a mask (Pin)