2013-10-16 2:55 AM
Has anybody here gotten the STM32F205 ULPI HS USB to work with SMSC USB3317?.
or for that matter any of the SMSC USB transceivers? Thanks,2013-10-16 6:23 AM
I've seen the USB3300 used on several F4 boards.
2013-10-16 8:35 AM
Looks like they are still using the ISP1705 (EOL now) on their F407 Eval boards.
Have you seen the USB3300 used on STM32 prototype boards ?2013-10-16 9:54 AM
Have you seen the USB3300 used on STM32 prototype boards ?
http://www.st.com/web/catalog/tools/FM116/SC959/SS1532/PF259093?icmp=stm32f4pr_pron_p3436s_sep2013#
Also on the RedDragon407