2015-03-20 2:57 AM
Dears all,
I'm looking for HAL SD (and SDIO, SDMMC) pdf description for STM32F2 but: No HAL description exist for STM32F2xx. In STM32F4 HAL description, no information about SD and SDMMC (and sdio). Could someone point me a web link to these pdf. Thanks in advance Oli2015-10-12 5:17 AM
ran into the same problem. Try the F7 HAL document. It has a section on SD HAL and I hope the API would be the same for portability.
ST documentation could use significant improvement2015-10-12 5:31 AM
> In STM32F4 HAL description, no information about SD and SDMMC (and sdio).
http://www.st.com/st-web-ui/static/active/en/resource/technical/document/user_manual/DM00105879.pdf
, see section 56 for SD information.2015-10-13 3:30 AM
Hi guys,
STM32F2 HAL description user manual (UM1940) is under finalization and first version will be available next week on ST web.
-Shahrzad-
2015-10-23 4:02 AM
Hi,
Description of STMF2xx HAL drivershttp://www.st.com/st-web-ui/static/active/en/resource/technical/document/user_manual/DM00223149.pdf
is available on ST web. -Shahrzad-