cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F2, 5V open drain pin

vindhyachal
Associate II
Posted on April 23, 2015 at 14:56

1. I am using stm32f205.

2. MCU is powered by 3.3V.

3. Another ic pin is driven by 5V logic or (Vih = 0.7*VDD = 3.5V)

4. Can I set pin of STM32F2 as open drain & connect 5V by pull up to it.

5. Datasheet of MCU says that they are not true open drain pins.
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Posted on April 24, 2015 at 03:03

You've enumerated some points, was there a question?

The Open-Drain mode only enables one transistor, the one that clamps to ground. In the high output mode the pin floats, to whatever supply you pull it too, the current will be limited by the resistor. This may also create a potential divider where the output high voltage is less than 5V.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..