cancel
Showing results for 
Search instead for 
Did you mean: 

STM32f1xx family MPU table?

Mikexx
Associate II
Posted on July 20, 2016 at 00:51

The Memory Protection Unit (MPU) is a feature that is only implemented in some members of the STM32F1xx family.

Is there a simple table which I can peruse to determine which members have the MPU, and which don't have this feature?
This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
slimen
Senior
Posted on July 20, 2016 at 10:36

Hi,

You should refer to the corresponding device datasheet to see if the MPU feature is present in the STM32 type you are using.

You can refer to this

http://www.st.com/content/ccc/resource/technical/document/programming_manual/5b/ca/8d/83/56/7f/40/08/CD00228163.pdf/files/CD00228163.pdf/jcr:content/translations/en.CD00228163.pdf

 , it can help you in section 4.2 Memory protection unit (MPU)

Regards

Mikexx
Associate II
Posted on July 20, 2016 at 14:02

Posted on July 20, 2016 at 15:35

Top post responses...

How many F1 chips do you need to use? Can you use other critical parameters to pare down the list a bit?

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..