cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F10xxx firmware library V2.0.1

tdropka
Associate
Posted on January 24, 2014 at 18:46

Is the STM32F10xxx firmware library (FWLib) version 2.0.1 available anywhere? The ''STM32 Legacy Firmware Libraries'' page starts at 2.0.3, but I need to port an application from 2.0.1 to StdPeriph_Lib v3.5.0 and I need to see what modifications the original developer made to 2.0.1. There were enough changes between 2.0.1 and 2.0.3 that I can't tell which ones were his.

Thanks, Tom
This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Posted on January 24, 2014 at 20:37

These are the V2.0.1 files I have repackaged

________________

Attachments :

STM32F10xFWLib_V2.0.1.zip : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I0qs&d=%2Fa%2F0X0000000beS%2Fsf1HAAJURsKE5hzjN_LRYwszkKQhHdkKSCa1pX579hk&asPdf=false
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
tdropka
Associate
Posted on January 24, 2014 at 20:45

Thank you very much, clive1. That was exactly what I needed.

Tom