2013-12-24 2:16 AM
Hello Guys,
I tried to put STM32F107VCT6 on STM32F103VCT6 board, I got this error when I tried to upload / erase the flash, any ideas why ? Thanks * JLink Info: Could not measure total IR len. TDO is constant high. **JLink Warning: CPU core not found. * JLink Info: Could not measure total IR len. TDO is constant high. * JLink Info: Could not measure total IR len. TDO is constant high. * JLink Info: Could not measure total IR len. TDO is constant high. * JLink Info: Could not measure total IR len. TDO is constant high. * JLink Info: Could not measure total IR len. TDO is constant high. * JLink Info: Could not measure total IR len. TDO is constant high. * JLink Info: Could not measure total IR len. TDO is constant high. * JLink Info: Could not measure total IR len. TDO is constant high. * JLink Info: Could not measure total IR len. TDO is constant high. * JLink Info: Could not measure total IR len. TDO is constant high. * JLink Info: Could not measure total IR len. TDO is constant high. * JLink Info: Could not measure total IR len. TDO is constant high. * JLink Info: Could not measure total IR len. TDO is constant high. * JLink Info: Could not measure total IR len. TDO is constant high. * JLink Info: Could not measure total IR len. TDO is constant high. * JLink Info: Could not measure total IR len. TDO is constant high. * JLink Info: Could not measure total IR len. TDO is constant high. * JLink Info: Could not measure total IR len. TDO is constant high. * JLink Info: Could not measure total IR len. TDO is constant high. * JLink Info: Could not measure total IR len. TDO is constant high. * JLink Info: Could not measure total IR len. TDO is constant high. * JLink Info: Could not measure total IR len. TDO is constant high. * JLink Info: Could not measure total IR len. TDO is constant high. * JLink Info: Could not measure total IR len. TDO is constant high. * JLink Info: Could not measure total IR len. TDO is constant high. * JLink Info: Could not measure total IR len. TDO is constant high. * JLink Info: Could not measure total IR len. TDO is constant high. * JLink Info: Could not measure total IR len. TDO is constant high. * JLink Info: Could not measure total IR len. TDO is constant high. * JLink Info: Could not measure total IR len. TDO is constant high. * JLink Info: Could not measure total IR len. TDO is constant high. * JLink Info: Could not measure total IR len. TDO is constant high. * JLink Info: Could not measure total IR len. TDO is constant high. * JLink Info: Could not measure total IR len. TDO is constant high. * JLink Info: Could not measure total IR len. TDO is constant high. * JLink Info: Could not measure total IR len. TDO is constant high. * JLink Info: Could not measure total IR len. TDO is constant high. * JLink Info: Could not measure total IR len. TDO is constant high. * JLink Info: Could not measure total IR len. TDO is constant high. * JLink Info: Could not measure total IR len. TDO is constant high. * JLink Info: Could not measure total IR len. TDO is constant high. * JLink Info: Could not measure total IR len. TDO is constant high. * JLink Info: Could not measure total IR len. TDO is constant high. * JLink Info: Could not measure total IR len. TDO is constant high. * JLink Info: Could not measure total IR len. TDO is constant high. * JLink Info: Could not measure total IR len. TDO is constant high. * JLink Info: Could not measure total IR len. TDO is constant high. * JLink Info: Could not measure total IR len. TDO is constant high. * JLink Info: Could not measure total IR len. TDO is constant high. * JLink Info: Could not measure total IR len. TDO is constant high. ***JLink Error: Wrong AHB ID (15:3). Expected 0x04770001 (Mask 0x0FFFFF0F), Found 0xFFFFFFFF2013-12-24 4:10 PM
it's working already, I resoldered it, could be dry join or something like that,
thanks for helping SEGGER J-Link Commander V4.24c ('?' for help) Compiled Mar 4 2011 20:04:53 DLL version V4.24c, compiled Mar 4 2011 20:04:34 Firmware: J-Link ARM V8 compiled Jan 31 2018 18:34:52 Hardware: V8.00 S/N: 20080643 Feature(s): RDI,FlashDL,FlashBP,JFlash,GDBFull J-Link>power on J-Link>st VTarget=3.351V ITarget=77mA TCK=1 TDI=0 TDO=1 TMS=0 TRES=1 TRST=1 Supported JTAG speeds: - 48 MHz/n, (n>=4). => 12000kHz, 9600kHz, 8000kHz, ... - Adaptive clocking J-Link>hwinfo HWInfo[00] = Target power is enabled HWInfo[02] = 77mA (ITarget) HWInfo[03] = 2056mA (ITargetPeak) HWInfo[04] = 90mA (ITargetPeakOperation) HWInfo[10] = 0ms (ITargetMaxTime0) HWInfo[11] = 1ms (ITargetMaxTime1) HWInfo[12] = 2ms (ITargetMaxTime2) J-Link>st VTarget=3.351V ITarget=77mA TCK=1 TDI=0 TDO=1 TMS=0 TRES=1 TRST=1 Supported JTAG speeds: - 48 MHz/n, (n>=4). => 12000kHz, 9600kHz, 8000kHz, ... - Adaptive clocking J-Link>r Info: TotalIRLen = 9, IRPrint = 0x0011 Reset delay: 0 ms Reset type NORMAL: Resets core & peripherals via SYSRESETREQ & VECTRESET bit. Info: TotalIRLen = 9, IRPrint = 0x0011 Info: Found Cortex-M3 r1p1, Little endian. Info: TPIU fitted. Info: ETM fitted. Info: FPUnit: 6 code (BP) slots and 2 literal slots J-Link>r Reset delay: 0 ms Reset type NORMAL: Resets core & peripherals via SYSRESETREQ & VECTRESET bit. Info: TotalIRLen = 9, IRPrint = 0x0011 Info: Found Cortex-M3 r1p1, Little endian. Info: TPIU fitted. Info: ETM fitted. Info: FPUnit: 6 code (BP) slots and 2 literal slots J-Link>2013-12-24 6:55 PM
Glad you got it working.
Yes, I had looked at the schematic PDF, I checked all the pins, I couldn't see any nets connected to Pin 94, but can't DRC or check the netlist from the supplied drawing. R13 looked to be marked as 220 Ohm. Not sure I established why NJTRST and NRST were connected in this fashion. NRST has it's 10K pull up as R3, so assumed the ''do not fit'' related to R12We’re moving the ST Community to a new platform to give you a better and more reliable community experience.