2013-12-24 2:16 AM
Hello Guys,
I tried to put STM32F107VCT6 on STM32F103VCT6 board, I got this error when I tried to upload / erase the flash, any ideas why ? Thanks * JLink Info: Could not measure total IR len. TDO is constant high. **JLink Warning: CPU core not found. * JLink Info: Could not measure total IR len. TDO is constant high. * JLink Info: Could not measure total IR len. TDO is constant high. * JLink Info: Could not measure total IR len. TDO is constant high. * JLink Info: Could not measure total IR len. TDO is constant high. * JLink Info: Could not measure total IR len. TDO is constant high. * JLink Info: Could not measure total IR len. TDO is constant high. * JLink Info: Could not measure total IR len. TDO is constant high. * JLink Info: Could not measure total IR len. TDO is constant high. * JLink Info: Could not measure total IR len. TDO is constant high. * JLink Info: Could not measure total IR len. TDO is constant high. * JLink Info: Could not measure total IR len. TDO is constant high. * JLink Info: Could not measure total IR len. TDO is constant high. * JLink Info: Could not measure total IR len. TDO is constant high. * JLink Info: Could not measure total IR len. TDO is constant high. * JLink Info: Could not measure total IR len. TDO is constant high. * JLink Info: Could not measure total IR len. TDO is constant high. * JLink Info: Could not measure total IR len. TDO is constant high. * JLink Info: Could not measure total IR len. TDO is constant high. * JLink Info: Could not measure total IR len. TDO is constant high. * JLink Info: Could not measure total IR len. TDO is constant high. * JLink Info: Could not measure total IR len. TDO is constant high. * JLink Info: Could not measure total IR len. TDO is constant high. * JLink Info: Could not measure total IR len. TDO is constant high. * JLink Info: Could not measure total IR len. TDO is constant high. * JLink Info: Could not measure total IR len. TDO is constant high. * JLink Info: Could not measure total IR len. TDO is constant high. * JLink Info: Could not measure total IR len. TDO is constant high. * JLink Info: Could not measure total IR len. TDO is constant high. * JLink Info: Could not measure total IR len. TDO is constant high. * JLink Info: Could not measure total IR len. TDO is constant high. * JLink Info: Could not measure total IR len. TDO is constant high. * JLink Info: Could not measure total IR len. TDO is constant high. * JLink Info: Could not measure total IR len. TDO is constant high. * JLink Info: Could not measure total IR len. TDO is constant high. * JLink Info: Could not measure total IR len. TDO is constant high. * JLink Info: Could not measure total IR len. TDO is constant high. * JLink Info: Could not measure total IR len. TDO is constant high. * JLink Info: Could not measure total IR len. TDO is constant high. * JLink Info: Could not measure total IR len. TDO is constant high. * JLink Info: Could not measure total IR len. TDO is constant high. * JLink Info: Could not measure total IR len. TDO is constant high. * JLink Info: Could not measure total IR len. TDO is constant high. * JLink Info: Could not measure total IR len. TDO is constant high. * JLink Info: Could not measure total IR len. TDO is constant high. * JLink Info: Could not measure total IR len. TDO is constant high. * JLink Info: Could not measure total IR len. TDO is constant high. * JLink Info: Could not measure total IR len. TDO is constant high. * JLink Info: Could not measure total IR len. TDO is constant high. * JLink Info: Could not measure total IR len. TDO is constant high. * JLink Info: Could not measure total IR len. TDO is constant high. ***JLink Error: Wrong AHB ID (15:3). Expected 0x04770001 (Mask 0x0FFFFF0F), Found 0xFFFFFFFF2013-12-24 5:00 AM
I haven't done the analysis on the pins, but would seem it's just not working, or incorrectly orientated. A secondary test would be via a serial port connected to USART1 and BOOT0 High, and trying to send 0x7F at 9600 8E1, and confirming an 0x79 response.
2013-12-24 7:25 AM
Here's the schematic with STM32F103
2013-12-24 7:28 AM
2013-12-24 7:39 AM
From J-commander :
SEGGER J-Link Commander V4.24c ('?' for help) Compiled Mar 4 2011 20:04:53 DLL version V4.24c, compiled Mar 4 2011 20:04:34 Firmware: J-Link ARM V8 compiled Jan 31 2018 18:34:52 Hardware: V8.00 S/N: 20080643 Feature(s): RDI,FlashDL,FlashBP,JFlash,GDBFull J-Link>r WARNING: CPU core not found. ****** Error: Supply voltage too low (1 Volt is required, Measured: 0.0 Volt). Please check target power. Reset delay: 0 ms Reset type UNKNOWN: ??? J-Link>power on J-Link>r WARNING: CPU core not found. Reset delay: 0 ms Reset type UNKNOWN: ??? WARNING: CPU core not found. J-Link>hwinfo HWInfo[00] = Target power is enabled HWInfo[02] = 38mA (ITarget) HWInfo[03] = 1959mA (ITargetPeak) HWInfo[04] = 51mA (ITargetPeakOperation) HWInfo[10] = 0ms (ITargetMaxTime0) HWInfo[11] = 1ms (ITargetMaxTime1) HWInfo[12] = 1ms (ITargetMaxTime2) J-Link>st VTarget=3.351V ITarget=38mA TCK=1 TDI=0 TDO=1 TMS=0 TRES=1 TRST=1 Supported JTAG speeds: - 48 MHz/n, (n>=4). => 12000kHz, 9600kHz, 8000kHz, ... - Adaptive clocking J-Link>halt ****** Error: Can not read register 8 (CPSR) while CPU is running ****** Error: Can not read register 9 (R15 (PC)) while CPU is running PC: (R15) = 00000000, CPSR = 00000000 (Unknown mode, ARM) ****** Error: Can not read register 7 (R7) while CPU is running ****** Error: Can not read register 6 (R6) while CPU is running ****** Error: Can not read register 5 (R5) while CPU is running ****** Error: Can not read register 4 (R4) while CPU is running ****** Error: Can not read register 3 (R3) while CPU is running ****** Error: Can not read register 2 (R2) while CPU is running ****** Error: Can not read register 1 (R1) while CPU is running ****** Error: Can not read register 0 (R0) while CPU is running R0 = 00000000, R1 = 00000000, R2 = 00000000, R3 = 00000000 R4 = 00000000, R5 = 00000000, R6 = 00000000, R7 = 00000000 ****** Error: Can not read register 14 (R12_USR) while CPU is running ****** Error: Can not read register 13 (R11_USR) while CPU is running ****** Error: Can not read register 12 (R10_USR) while CPU is running ****** Error: Can not read register 11 (R9_USR) while CPU is running ****** Error: Can not read register 10 (R8_USR) while CPU is running USR: R8 =00000000, R9 =00000000, R10=00000000, R11 =00000000, R12 =00000000 ****** Error: Can not read register 16 (R14_USR) while CPU is running ****** Error: Can not read register 15 (R13_USR) while CPU is running R13=00000000, R14=00000000 ****** Error: Can not read register 22 (R12_FIQ) while CPU is running ****** Error: Can not read register 21 (R11_FIQ) while CPU is running ****** Error: Can not read register 20 (R10_FIQ) while CPU is running ****** Error: Can not read register 19 (R9_FIQ) while CPU is running ****** Error: Can not read register 18 (R8_FIQ) while CPU is running FIQ: R8 =00000000, R9 =00000000, R10=00000000, R11 =00000000, R12 =00000000 ****** Error: Can not read register 17 (SPSR_FIQ) while CPU is running ****** Error: Can not read register 24 (R14_FIQ) while CPU is running ****** Error: Can not read register 23 (R13_FIQ) while CPU is running R13=00000000, R14=00000000, SPSR=00000000 ****** Error: Can not read register 25 (SPSR_SVC) while CPU is running ****** Error: Can not read register 27 (R14_SVC) while CPU is running ****** Error: Can not read register 26 (R13_SVC) while CPU is running SVC: R13=00000000, R14=00000000, SPSR=00000000 ****** Error: Can not read register 28 (SPSR_ABT) while CPU is running ****** Error: Can not read register 30 (R14_ABT) while CPU is running ****** Error: Can not read register 29 (R13_ABT) while CPU is running ABT: R13=00000000, R14=00000000, SPSR=00000000 ****** Error: Can not read register 31 (SPSR_IRQ) while CPU is running ****** Error: Can not read register 33 (R14_IRQ) while CPU is running ****** Error: Can not read register 32 (R13_IRQ) while CPU is running IRQ: R13=00000000, R14=00000000, SPSR=00000000 ****** Error: Can not read register 34 (SPSR_UND) while CPU is running ****** Error: Can not read register 36 (R14_UND) while CPU is running ****** Error: Can not read register 35 (R13_UND) while CPU is running UND: R13=00000000, R14=00000000, SPSR=00000000 J-Link>2013-12-24 7:46 AM
Ok, so you have both RS232 and USB. You'll want to try the serial port test with BOOT0 high, and if the USB comes up in DFU mode. If these don't work the chip is not functioning, no amount of banging on the JLink will resolve this.
Your second test doesn't even appear to be powering the board. Check the 3V3 rail, and 5V from the JLINK. Do not understand the purpose of R13 coupling NJTRST and NRST2013-12-24 8:05 AM
Pin 94 (BOOT0) doesn't appear to be connected to anything.
2013-12-24 2:34 PM
2013-12-24 2:51 PM
I checked it with voltmeter, pin 94 is connected properly to 10K resistor (R4),
do you recommend me to undo R13 ? Have you seen the schematic ?2013-12-24 2:59 PM
without R13 and boot0 = 0 :
SEGGER J-Link Commander V4.24c ('?' for help) Compiled Mar 4 2011 20:04:53 DLL version V4.24c, compiled Mar 4 2011 20:04:34 Firmware: J-Link ARM V8 compiled Jan 31 2018 18:34:52 Hardware: V8.00 S/N: 20080643 Feature(s): RDI,FlashDL,FlashBP,JFlash,GDBFull J-Link>power on J-Link>r Info: Could not measure total IR len. TDO is constant high. WARNING: CPU core not found. Reset delay: 0 ms Reset type UNKNOWN: ??? Info: Could not measure total IR len. TDO is constant high. WARNING: CPU core not found. J-Link>st VTarget=3.351V ITarget=45mA TCK=1 TDI=0 TDO=1 TMS=0 TRES=1 TRST=1 Supported JTAG speeds: - 48 MHz/n, (n>=4). => 12000kHz, 9600kHz, 8000kHz, ... - Adaptive clocking J-Link>We’re moving the ST Community to a new platform to give you a better and more reliable community experience.