2013-12-24 02:16 AM
Hello Guys,
I tried to put STM32F107VCT6 on STM32F103VCT6 board, I got this error when I tried to upload / erase the flash, any ideas why ? Thanks * JLink Info: Could not measure total IR len. TDO is constant high. **JLink Warning: CPU core not found. * JLink Info: Could not measure total IR len. TDO is constant high. * JLink Info: Could not measure total IR len. TDO is constant high. * JLink Info: Could not measure total IR len. TDO is constant high. * JLink Info: Could not measure total IR len. TDO is constant high. * JLink Info: Could not measure total IR len. TDO is constant high. * JLink Info: Could not measure total IR len. TDO is constant high. * JLink Info: Could not measure total IR len. TDO is constant high. * JLink Info: Could not measure total IR len. TDO is constant high. * JLink Info: Could not measure total IR len. TDO is constant high. * JLink Info: Could not measure total IR len. TDO is constant high. * JLink Info: Could not measure total IR len. TDO is constant high. * JLink Info: Could not measure total IR len. TDO is constant high. * JLink Info: Could not measure total IR len. TDO is constant high. * JLink Info: Could not measure total IR len. TDO is constant high. * JLink Info: Could not measure total IR len. TDO is constant high. * JLink Info: Could not measure total IR len. TDO is constant high. * JLink Info: Could not measure total IR len. TDO is constant high. * JLink Info: Could not measure total IR len. TDO is constant high. * JLink Info: Could not measure total IR len. TDO is constant high. * JLink Info: Could not measure total IR len. TDO is constant high. * JLink Info: Could not measure total IR len. TDO is constant high. * JLink Info: Could not measure total IR len. TDO is constant high. * JLink Info: Could not measure total IR len. TDO is constant high. * JLink Info: Could not measure total IR len. TDO is constant high. * JLink Info: Could not measure total IR len. TDO is constant high. * JLink Info: Could not measure total IR len. TDO is constant high. * JLink Info: Could not measure total IR len. TDO is constant high. * JLink Info: Could not measure total IR len. TDO is constant high. * JLink Info: Could not measure total IR len. TDO is constant high. * JLink Info: Could not measure total IR len. TDO is constant high. * JLink Info: Could not measure total IR len. TDO is constant high. * JLink Info: Could not measure total IR len. TDO is constant high. * JLink Info: Could not measure total IR len. TDO is constant high. * JLink Info: Could not measure total IR len. TDO is constant high. * JLink Info: Could not measure total IR len. TDO is constant high. * JLink Info: Could not measure total IR len. TDO is constant high. * JLink Info: Could not measure total IR len. TDO is constant high. * JLink Info: Could not measure total IR len. TDO is constant high. * JLink Info: Could not measure total IR len. TDO is constant high. * JLink Info: Could not measure total IR len. TDO is constant high. * JLink Info: Could not measure total IR len. TDO is constant high. * JLink Info: Could not measure total IR len. TDO is constant high. * JLink Info: Could not measure total IR len. TDO is constant high. * JLink Info: Could not measure total IR len. TDO is constant high. * JLink Info: Could not measure total IR len. TDO is constant high. * JLink Info: Could not measure total IR len. TDO is constant high. * JLink Info: Could not measure total IR len. TDO is constant high. * JLink Info: Could not measure total IR len. TDO is constant high. * JLink Info: Could not measure total IR len. TDO is constant high. * JLink Info: Could not measure total IR len. TDO is constant high. ***JLink Error: Wrong AHB ID (15:3). Expected 0x04770001 (Mask 0x0FFFFF0F), Found 0xFFFFFFFF2013-12-24 04:10 PM
it's working already, I resoldered it, could be dry join or something like that,
thanks for helping SEGGER J-Link Commander V4.24c ('?' for help) Compiled Mar 4 2011 20:04:53 DLL version V4.24c, compiled Mar 4 2011 20:04:34 Firmware: J-Link ARM V8 compiled Jan 31 2018 18:34:52 Hardware: V8.00 S/N: 20080643 Feature(s): RDI,FlashDL,FlashBP,JFlash,GDBFull J-Link>power on J-Link>st VTarget=3.351V ITarget=77mA TCK=1 TDI=0 TDO=1 TMS=0 TRES=1 TRST=1 Supported JTAG speeds: - 48 MHz/n, (n>=4). => 12000kHz, 9600kHz, 8000kHz, ... - Adaptive clocking J-Link>hwinfo HWInfo[00] = Target power is enabled HWInfo[02] = 77mA (ITarget) HWInfo[03] = 2056mA (ITargetPeak) HWInfo[04] = 90mA (ITargetPeakOperation) HWInfo[10] = 0ms (ITargetMaxTime0) HWInfo[11] = 1ms (ITargetMaxTime1) HWInfo[12] = 2ms (ITargetMaxTime2) J-Link>st VTarget=3.351V ITarget=77mA TCK=1 TDI=0 TDO=1 TMS=0 TRES=1 TRST=1 Supported JTAG speeds: - 48 MHz/n, (n>=4). => 12000kHz, 9600kHz, 8000kHz, ... - Adaptive clocking J-Link>r Info: TotalIRLen = 9, IRPrint = 0x0011 Reset delay: 0 ms Reset type NORMAL: Resets core & peripherals via SYSRESETREQ & VECTRESET bit. Info: TotalIRLen = 9, IRPrint = 0x0011 Info: Found Cortex-M3 r1p1, Little endian. Info: TPIU fitted. Info: ETM fitted. Info: FPUnit: 6 code (BP) slots and 2 literal slots J-Link>r Reset delay: 0 ms Reset type NORMAL: Resets core & peripherals via SYSRESETREQ & VECTRESET bit. Info: TotalIRLen = 9, IRPrint = 0x0011 Info: Found Cortex-M3 r1p1, Little endian. Info: TPIU fitted. Info: ETM fitted. Info: FPUnit: 6 code (BP) slots and 2 literal slots J-Link>2013-12-24 06:55 PM
Glad you got it working.
Yes, I had looked at the schematic PDF, I checked all the pins, I couldn't see any nets connected to Pin 94, but can't DRC or check the netlist from the supplied drawing. R13 looked to be marked as 220 Ohm. Not sure I established why NJTRST and NRST were connected in this fashion. NRST has it's 10K pull up as R3, so assumed the ''do not fit'' related to R12