cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F105 SPI2 issue

nps
Associate II
Posted on March 13, 2015 at 19:06

Hello all,

I faced problems with SPI2. First I interfaced a graphic LCD on SPI bus and could not get to working properly, though it works well on an Atmel 8 bit controller. Spent more than 3 weeks without much luck. Now I interfaced Spansion flash memory. This chip supports reading manufacturer and device identification. When queried it must return 0x15. On STM32F105 returns 02, whereas 0x15 (correct value) is returned on 8 bit controller. Checked clock polarity. Here is my SPI initialization code. Any suggestions please? Thank you.

    GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;

    GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF_PP;

    GPIO_InitStructure.GPIO_Pin = GPIO_Pin_13 | GPIO_Pin_14 | GPIO_Pin_15;    

    GPIO_Init(GPIOB, &GPIO_InitStructure);

    SPI_InitStructure.SPI_Mode = SPI_Mode_Master;

    SPI_InitStructure.SPI_Direction = SPI_Direction_2Lines_FullDuplex;

    SPI_InitStructure.SPI_DataSize = SPI_DataSize_8b;

    SPI_InitStructure.SPI_NSS = SPI_NSS_Soft;

    SPI_InitStructure.SPI_CPOL = SPI_CPOL_High;

    SPI_InitStructure.SPI_CPHA = SPI_CPHA_2Edge;        //

    SPI_InitStructure.SPI_BaudRatePrescaler = SPI_BaudRatePrescaler_64;

    SPI_InitStructure.SPI_FirstBit = SPI_FirstBit_MSB;

    SPI_Init(SPI2, &SPI_InitStructure);    // currently used SPI on this board

    SPI_Cmd(SPI2, ENABLE);

#stm32f105-spi2
This discussion is locked. Please start a new topic to ask your question.
5 REPLIES 5
Posted on March 13, 2015 at 20:06

The F1 parts expect MISO pin to be configured in INPUT mode on the Master, not AF

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Posted on March 13, 2015 at 20:24

This is for an F4, but these worked with the SPI NOR Flash I was testing

/* configure SPI2 in Mode 0
* CPOL = 0 --> clock is low when idle
* CPHA = 0 --> data is sampled at the first edge
*/
SPI_InitStruct.SPI_Direction = SPI_Direction_2Lines_FullDuplex; // set to full duplex mode, seperate MOSI and MISO lines
SPI_InitStruct.SPI_Mode = SPI_Mode_Master; // transmit in master mode, NSS pin has to be always high
SPI_InitStruct.SPI_DataSize = SPI_DataSize_8b; // one packet of data is 8 bits wide
SPI_InitStruct.SPI_CPOL = SPI_CPOL_Low; // clock is low when idle
SPI_InitStruct.SPI_CPHA = SPI_CPHA_1Edge; // data sampled at first edge
SPI_InitStruct.SPI_NSS = SPI_NSS_Soft | SPI_NSSInternalSoft_Set; // set the NSS management to internal and pull internal NSS high
SPI_InitStruct.SPI_BaudRatePrescaler = SPI_BaudRatePrescaler_2; // SPI frequency is APB2 frequency / 4
SPI_InitStruct.SPI_FirstBit = SPI_FirstBit_MSB;// data is transmitted MSB first
SPI_Init(SPI2, &SPI_InitStruct);
SPI_Cmd(SPI2, ENABLE); // enable SPI2

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
nps
Associate II
Posted on March 14, 2015 at 02:01

Hi clive1,

Thanks for the reply. Yes I tried all possible combinations. Here is the modified code. The funny thing is, we did not face much problems on an stm32f103. LCD does not have a read facility so only MOSI was used. The other difference is SPI2. In the f103 board we used SPI1. Is there a difference between the two? We are also using usart3 in UART mode. Please help resolve this once and for all. The board is a two layer board and UART1 and 3 work well. Thanks for your help.

nps
Associate II
Posted on March 14, 2015 at 02:05

Sorry I think I missed to add the code. Here it is. This is also returning 02 instead of 0x15

    GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;

    GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF_PP;

    GPIO_InitStructure.GPIO_Pin = GPIO_Pin_13 | GPIO_Pin_15;        // SPI2

    GPIO_Init(GPIOB, &GPIO_InitStructure);

//    GPIO_InitStructure.GPIO_Mode = GPIO_Mode_IN_FLOATING;        // MISO

//    GPIO_InitStructure.GPIO_Pin = GPIO_Pin_14;

//    GPIO_Init(GPIOB, &GPIO_InitStructure);

    SPI_InitStructure.SPI_Mode = SPI_Mode_Master;

    SPI_InitStructure.SPI_Direction = SPI_Direction_2Lines_FullDuplex;

    SPI_InitStructure.SPI_DataSize = SPI_DataSize_8b;

    SPI_InitStructure.SPI_NSS = SPI_NSS_Soft | SPI_NSSInternalSoft_Set;

    SPI_InitStructure.SPI_CPOL = SPI_CPOL_Low;

    SPI_InitStructure.SPI_CPHA = SPI_CPHA_1Edge;        //

    SPI_InitStructure.SPI_BaudRatePrescaler = SPI_BaudRatePrescaler_64;

    SPI_InitStructure.SPI_FirstBit = SPI_FirstBit_MSB;

    SPI_Init(SPI2, &SPI_InitStructure);    // currently used SPI on this board

    SPI_Cmd(SPI2, ENABLE);

nps
Associate II
Posted on March 14, 2015 at 03:16

Hi Clive1,

Thanks for the help. The code is working now. The mistake was, waiting for TX complete and not RXNE. I thought I used RXNE hence did not take a closer look. I made MISO input with pull-up. Thank you once again.