2011-09-27 11:12 PM
Hi,
Im trying to get the usart2 working but for some reason I get random corrupted data when I send message to the STM32F103T8. I can send messages from the STM32 to the computer without any corrupted bytes but not the other way around.The usart2 is piping the received messages to a DMA. I've activated the usart2 in the following way: DMA_DeInit(DMA1_Channel6); DMA_StructInit(&DMA_InitStructure); DMA_InitStructure.DMA_PeripheralBaseAddr = USART2_DR_Base; DMA_InitStructure.DMA_MemoryBaseAddr = (uint32_t)gRXBuf2; //Define in usart2.h DMA_InitStructure.DMA_DIR = DMA_DIR_PeripheralSRC; DMA_InitStructure.DMA_MemoryInc = DMA_MemoryInc_Enable; DMA_InitStructure.DMA_PeripheralInc = DMA_PeripheralInc_Disable; DMA_InitStructure.DMA_BufferSize = RX_BUF_SIZE2; //Define in usart2.h DMA_InitStructure.DMA_Mode = DMA_Mode_Circular; DMA_InitStructure.DMA_M2M = DMA_M2M_Disable; DMA_InitStructure.DMA_Priority = DMA_Priority_VeryHigh; DMA_Init( DMA1_Channel6, &DMA_InitStructure );USART_InitStructure2.USART_BaudRate = 4800;
USART_InitStructure2.USART_WordLength = USART_WordLength_8b;
USART_InitStructure2.USART_StopBits = USART_StopBits_1;
USART_InitStructure2.USART_Parity = USART_Parity_No;
USART_InitStructure2.USART_HardwareFlowControl = USART_HardwareFlowControl_None;
USART_InitStructure2.USART_Mode = USART_Mode_Rx | USART_Mode_Tx;
/* Configure USART2 */
USART_Init(USART2, &USART_InitStructure2);
/* Enable USART2 Receive and Transmit interrupts */ USART_ITConfig(USART2, USART_IT_TC, ENABLE); // Enable USART2 Receive DMA requests USART_DMACmd(USART2, USART_DMAReq_Rx, ENABLE); // Enable DMA1 USART RX channel DMA_Cmd(DMA1_Channel6, ENABLE); // Enable USART2 USART_Cmd(USART2, ENABLE);I have also enabled the usart2 clock as following: RCC_APB1PeriphClockCmd(RCC_APB1Periph_USART2, ENABLE);And finally enabled the usart2 interrupt: NVIC_InitStructure.NVIC_IRQChannel = USART2_IRQn; NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 0; NVIC_InitStructure.NVIC_IRQChannelSubPriority = 0; NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE; NVIC_Init(&NVIC_InitStructure);I've done a simple program which checks when new data have been added to the DMA memory where the received data is and send the exact same data back to the computer.Then i connect to the STM32 with the windows xp hyperterminal and sends some chars.For example if i send GPGGA, I might get back something like GP=GA or even worse like G?G, where some chars is ''.Does anyone have any idea what might be wrong? I would really appriciate the help.CheersMike #stm32-stm32f103-usart-corrupted2011-09-28 2:09 AM
''Does anyone have any idea what might be wrong?''
The usual reason is that your baud rate is not (quite) correct - have you checked with a scope to see exactly what baudrate the STM32 is actually using? Is the STM32 reporting any Framing errors?2011-09-28 4:25 AM
Thank you for such a fast answer.
Ive checked the framing error but it is never set, and I have also tested different baudrate but the same corruption occurred.I have more or less the same code for the USART1 but with dma channel 5 and it works perfectly.I recently discovered something which might be the problem.I gave the DMA the memory address for a buffer gRXBuf2 which basicly is defined as:volatile char gRXBuf2[RX_BUF_SIZE2];
The RX_BUF_SIZE2 is defined as 30. I belive that when the usart2 receives data it automaticly goes into the DMA memory, in this case the gRXBuf2, so for example if I send the message ''GPGGA'' then the buffer should look like: gRXBuf2[0] = 'G'gRXBuf2[
1] = '
P'
gRXBuf2[
2] = 'G'
gRXBuf2[
3] = 'G'
gRXBuf2[
4] = '
A'
So I tried to send the previous value in the buffer also.Something like this: USART2_transmit(''This: '', 6); USART2_transmit((char*)&gRXBuf2[gRXBufPtr2], 1); USART2_transmit(''\r\n'', 2); if(gRXBufPtr2>0) { USART2_transmit(''Prev: '', 6); USART2_transmit((char*)&gRXBuf2[gRXBufPtr2-1], 1); USART2_transmit(''\r\n'', 2); }And what I got when i only send a's is the following:This: êThis: aPrev: This: aPrev: �?This: <Prev: �?This:Prev: <This:Prev:This: €Prev:So even the previous value of the buffer changes. Ive searched through all the code and cant find any other places which are using the buffer, so is there maybe a problem with the dma?2011-09-28 5:16 AM
DMA_InitStructure.DMA_PeripheralDataSize = DMA_PeripheralDataSize_Byte;
DMA_InitStructure.DMA_MemoryDataSize = DMA_MemoryDataSize_Byte;2011-09-28 5:52 AM
I tried added:
DMA_InitStructure.DMA_PeripheralDataSize = DMA_PeripheralDataSize_Byte; DMA_InitStructure.DMA_MemoryDataSize = DMA_MemoryDataSize_Byte;but still same corruption of data.2011-09-28 6:42 AM
Does it work with polled (ie not IRQ or DMA) receive on the same USART?
2011-09-29 12:09 AM
Hi again,
Im sorry for the late answer but i tried what you said .I did a simple program like: while(1) { /* Loop until the USARTz Receive Data Register is not empty */ while(USART_GetFlagStatus(USART2, USART_FLAG_RXNE) == RESET) { } gRXBuf2[gRXBufPtr2++] = (USART_ReceiveData(USART2) & 0x7F); USART2_transmit((char*)&gRXBuf2[gRXBufPtr2-1], 1); if( gRXBufPtr2 == RX_BUF_SIZE2 ) { gRXBufPtr2 = 0; } }and it worked perfectly, so i assume that something is disturbing the dma channel?2011-10-03 11:26 PM
Just wanted to update this thread as I found the problem.
The problem was that I were on the limits of the memory on the MCU.So after I reduced some buffers everything worked perfectly.When you run out of memory, strange things start to happen.2012-06-12 5:17 AM
Hii
I had the same problem that you had, can you please tell me how to solve that, Actually I had (chr6dm) module which contain ARM Processor and in this module they used USART1 and now I need to use USART2 for another sensor, I think you also have the same module right ????2012-06-12 5:21 AM
I had forgot something what is the (
USART2_DR_Base
) that you used????