cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F103c8t6 external interrupt issue

sak hos
Associate III
Posted on August 21, 2017 at 17:03

hello,

i'm facing a strange issue, i'm using STM32F103c8t6 and i'm trying to use external interrupt (please take a look the configuration below), the issue is when i trigger the interruption only one time, the callback(HAL_GPIO_EXTI_Callback) is called twice in a row

does anyone have an idea about this

thank you

/*******************************************************************/

void MX_GPIO_Init(void)

{

GPIO_InitTypeDef GPIO_InitStruct;

/* GPIO Ports Clock Enable */

__HAL_RCC_GPIOC_CLK_ENABLE();

__HAL_RCC_GPIOD_CLK_ENABLE();

__HAL_RCC_GPIOA_CLK_ENABLE();

__HAL_RCC_GPIOB_CLK_ENABLE();

/*Configure GPIO pin : PA1 */

GPIO_InitStruct.Pin = GPIO_PIN_1;

GPIO_InitStruct.Mode = GPIO_MODE_IT_RISING;//GPIO_MODE_IT_RISING_FALLING;//GPIO_MODE_IT_RISING;

GPIO_InitStruct.Pull = GPIO_PULLDOWN;//GPIO_NOPULL;

HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);

/*Configure GPIO pins : PB0 PB12 PB15 PB5

PB6 PB7 PB8 PB9 */

GPIO_InitStruct.Pin = GPIO_PIN_0|GPIO_PIN_12|GPIO_PIN_15|GPIO_PIN_5

|GPIO_PIN_6|GPIO_PIN_7|GPIO_PIN_8|GPIO_PIN_9;

GPIO_InitStruct.Mode = GPIO_MODE_IT_RISING;

GPIO_InitStruct.Pull =GPIO_PULLDOWN; //GPIO_NOPULL;

HAL_GPIO_Init(GPIOB, &GPIO_InitStruct);

/* EXTI interrupt init*/

HAL_NVIC_SetPriority(EXTI0_IRQn, 0, 0);

HAL_NVIC_EnableIRQ(EXTI0_IRQn);

HAL_NVIC_SetPriority(EXTI1_IRQn, 0, 0);

HAL_NVIC_EnableIRQ(EXTI1_IRQn);

HAL_NVIC_SetPriority(EXTI9_5_IRQn, 0, 0);

HAL_NVIC_EnableIRQ(EXTI9_5_IRQn);

HAL_NVIC_SetPriority(EXTI15_10_IRQn, 0, 0);

HAL_NVIC_EnableIRQ(EXTI15_10_IRQn);

}

/********************************************************************************/

void HAL_GPIO_EXTI_Callback(uint16_t GPIO_Pin)

{

switch (GPIO_Pin)

{

case GPIO_PIN_0:/*BEGIN_END_OF_COMPETITION*/

MessageToBSent.Command=BEGIN_END_OF_COMPETITION;

MessageToBSent.DestinationAddress=BROADCAST_ADDRESS;

Send_Command_To_Modules (&MessageToBSent);

break;

case GPIO_PIN_1:/*START_COMPETITION or STOP_COMPETITION*/

if (StartStopCompetitionButtonLastValue==STOP_COMPETITION)

{

MessageToBSent.Command=START_COMPETITION;

MessageToBSent.DestinationAddress=TIMER_MODULE_ADDRESS;

Send_Command_To_Modules (&MessageToBSent);

StartStopCompetitionButtonLastValue=START_COMPETITION;

break;

}

}

}

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Posted on August 21, 2017 at 17:18

Review the IRQHandler code an how it qualifies, and clears the source.

IRQs can reenter if the last thing you do is clear the interrupt source. Do that after you've qualified the source, and before you call back into the HAL

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

View solution in original post

7 REPLIES 7
Posted on August 21, 2017 at 17:18

Review the IRQHandler code an how it qualifies, and clears the source.

IRQs can reenter if the last thing you do is clear the interrupt source. Do that after you've qualified the source, and before you call back into the HAL

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Bob Boys
Senior
Posted on August 21, 2017 at 17:34

Hello

Please give this a try:

http://www.keil.com/support/docs/3928.htm

 

Thanks

Bob Boys

on holidays in Ontario, Canada

waclawek.jan
Super User
Posted on August 21, 2017 at 18:11

If I understand Cube correctly, this is not the case.

/**

  * @brief  This function handles EXTI interrupt request.

  * @param  GPIO_Pin: Specifies the pins connected EXTI line

  * @retval None

  */

void HAL_GPIO_EXTI_IRQHandler(uint16_t GPIO_Pin)

{

  /* EXTI line interrupt detected */

  if(__HAL_GPIO_EXTI_GET_IT(GPIO_Pin) != RESET)

  {

    __HAL_GPIO_EXTI_CLEAR_IT(GPIO_Pin);

    HAL_GPIO_EXTI_Callback(GPIO_Pin);

  }

}

I'd suspect the interrupt source to be bouncy.

JW

waclawek.jan
Super User
Posted on August 21, 2017 at 19:41

The fact that an added flag clear *after* the bulk of ISR helped, confirms that it's not the case of late flag clear, but another interrupt arriving during that bulk.

JW

Posted on August 21, 2017 at 18:02

Hi Clive One ,

thanks it's done

i added __HAL_GPIO_EXTI_CLEAR_IT(GPIO_Pin); as mentioned bloow and now i have only one call of HAL_GPIO_EXTI_Callback(GPIO_Pin);

/******************************************/

void HAL_GPIO_EXTI_IRQHandler(uint16_t GPIO_Pin)

{

/* EXTI line interrupt detected */

if(__HAL_GPIO_EXTI_GET_IT(GPIO_Pin) != RESET)

{

__HAL_GPIO_EXTI_CLEAR_IT(GPIO_Pin);

HAL_GPIO_EXTI_Callback(GPIO_Pin);

__HAL_GPIO_EXTI_CLEAR_IT(GPIO_Pin); /*added*/

}

}

/******************************************/

but can you explain to me how can this happen

thanks a lot
Posted on August 21, 2017 at 19:36

Hello

This often looks just like a bouncy switch but it is not necessarily so.

The article I pointed to explains what is going on.

I came across this in one of the first STM32 processors about 10 years ago and someone encountered it a few weeks again.  In my case, I had a switch on a GPIO pin that generated an EXTI interrupt for a demo.

So, we made a new appnote explaining several solutions.

In the other case someone had, they were using GCC, the problem did not show up until some optimization was applied and the code got a lot smaller and the double interrupt appeared.  Using Keil and IAR, the problem showed immediatley with no optimization because these compilers happened to produce smaller code at the end of the interrupt handler.

It seems a lot of instructions near the end of the handler can make this problem disappear.

The best solution is apparently a dummy write is the solution across a wide variety of Cortex-M processors.

A DSB instruction can be effective too.

Bob

Posted on August 21, 2017 at 23:17

The best solution is apparently a dummy write is the solution across a wide variety of Cortex-M processors.

No; see attachment. Comments welcome.

The ARM guys tend to see their processor as the pinnacle of complexity, despising the surrounding circuitry.

JW

________________

Attachments :

m1.zip : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HyUB&d=%2Fa%2F0X0000000b8U%2FA9FxkgJZVZJRojPNCikGuo2uI0r_JvVL1kBHA0yFUNU&asPdf=false