Associate
September 30, 2013
Question
STM32f103 USB EP3 Interrupt Problem
- September 30, 2013
- 2 replies
- 1518 views
Posted on October 01, 2013 at 01:50
I am trying to configure the STM32F103 to be a device on the USB. I used the Virtual_COM_Port as a starting point. My USB config is as follows:
-ep0=control-ep1=bulk OUT-ep2=bulk IN-ep3=interruptEP0, EP1 and EP2 seem to be functioning correctly, but EP3 has issues. From my USB monitor I can see an IN packet being sent from the host to the device's EP3, but the device does not respond. I have a 22 bytes message ready to go This is strange because it is initialized the same as EP2 except SetEPType(ENDP3, EP_INTERRUPT);My Reset routine and descriptors are attached: