2011-08-12 10:55 AM
hello everybody
i'm using stm32f103rb to send and recieve data via USART
USART2&3 work completly but USART1 send data but can not recieve
i tried the keil's example but it didn't work
plz help me solve the problem
Thanck you
2011-08-12 12:47 PM
If you've eliminated software problems, perhaps you should be looking more carefully at your hardware/connection. I don't think your problem is solvable with the limited information furnished in the question.
Three USARTs are certainly workable on the 103. Check that you have the clocks enabled. Check that you have the USART, and Rx/Tx Enabled. If you have a Tx interrupt enabled, you'd better have some data to send. Check that you have the correct pins, mappings and settings. If you are remapping, make sure AFIO is clocking.2011-09-12 2:31 AM