2011-03-13 5:28 PM
STM32F103 - Timer issue after reset
2011-05-17 5:27 AM
Does anyone have an idea of what might be causing this?
Should we just guess at what you are doing wrong? or are you going to post the code?2011-05-17 5:27 AM
Guessing is good, code might be better...
void RCC_Configuration(void) { RCC_DeInit(); RCC_HSEConfig(RCC_HSE_ON); HSEStartUpStatus = RCC_WaitForHSEStartUp(); if (HSEStartUpStatus == SUCCESS) { FLASH_PrefetchBufferCmd(FLASH_PrefetchBuffer_Enable); FLASH_SetLatency(FLASH_Latency_2); RCC_HCLKConfig(RCC_SYSCLK_Div1); RCC_PCLK2Config(RCC_HCLK_Div1); RCC_PCLK1Config(RCC_HCLK_Div2); RCC_PLLConfig(RCC_PLLSource_HSE_Div1, RCC_PLLMul_9); RCC_PLLCmd(ENABLE); while (RCC_GetFlagStatus(RCC_FLAG_PLLRDY) == RESET) { } RCC_SYSCLKConfig(RCC_SYSCLKSource_PLLCLK); while(RCC_GetSYSCLKSource() != 0x08) { } } else { while (1) { } } /* Enable USART1, GPIOA, GPIOB, GPIOC and AFIO clocks */ RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOA | RCC_APB2Periph_GPIOB | RCC_APB2Periph_GPIOC | RCC_APB2Periph_AFIO, ENABLE); RCC_APB1PeriphClockCmd(RCC_APB1Periph_CAN1, ENABLE); RCC_APB2PeriphResetCmd(RCC_APB2Periph_GPIOA | RCC_APB2Periph_GPIOB | RCC_APB2Periph_GPIOC, DISABLE); } void initTimer(void) { TIM_TimeBaseInitTypeDef TimeBaseInit; TIM_OCInitTypeDef TIM_OCInitStructure; TimeBaseInit.TIM_Period = 35999; TimeBaseInit.TIM_Prescaler = 999; TimeBaseInit.TIM_ClockDivision = TIM_CKD_DIV1; TimeBaseInit.TIM_CounterMode = TIM_CounterMode_Up; TIM_TimeBaseInit(TIM2, &TimeBaseInit); TIM_OCInitStructure.TIM_OCMode = TIM_OCMode_Timing; TIM_OCInitStructure.TIM_OutputState = TIM_OutputState_Enable; TIM_OCInitStructure.TIM_Pulse = 6000; TIM_OCInitStructure.TIM_OCPolarity = TIM_OCPolarity_High; TIM_OC1Init(TIM2, &TIM_OCInitStructure); TIM_OC1PreloadConfig(TIM2, TIM_OCPreload_Disable); RCC_APB1PeriphClockCmd(RCC_APB1Periph_TIM2, ENABLE); TIM_ClearFlag(TIM2, TIM_IT_CC1); TIM_ClearITPendingBit(TIM2, TIM_IT_CC1); TIM_ITConfig(TIM2, TIM_IT_CC1, ENABLE); TIM_Cmd(TIM2, ENABLE); TIM_ClearITPendingBit(TIM2, TIM_IT_CC1); } void TIM2_IRQHandler() { if (TIM_GetITStatus(TIM2, TIM_IT_CC1) != RESET) { TIM_ClearITPendingBit(TIM2, TIM_IT_CC1); GPIO_WriteBit(GPIOC, GPIO_Pin_12, (BitAction) 1 - GPIO_ReadOutputDataBit(GPIOC, GPIO_Pin_12)); } }2011-05-17 5:27 AM
In void initTimer(void) try to call
RCC_APB1PeriphClockCmd(RCC_APB1Periph_TIM2, ENABLE); prior to init calls like TIM_OC1Init(TIM2, &TIM_OCInitStructure);
TIM_OC1PreloadConfig(TIM2, TIM_OCPreload_Disable);
2011-05-17 5:27 AM
Yes, you need to move
RCC_APB1PeriphClockCmd(RCC_APB1Periph_TIM2, ENABLE); to earlier in the init routine, so that the peripheral is functional while you are programming it's internal registers.2011-05-17 5:27 AM
That's done it, thanks a lot