2026-01-14 2:08 AM - last edited on 2026-01-14 2:16 AM by Andrew Neil
Hello everyone,
I am using SPI2 of STM32F103RCT6 to communicate with an AT45DB641E DataFlash device. I am trying to understand why the effective SPI data rate is significantly lower than what I expect based on the configured SPI clock.
Hardware setup
Test description
I am reading the status register of the AT45DB641E.
Once the read command is sent and SS is held low, the flash continuously outputs two status bytes as long as clock pulses are provided.
I measured the execution time of HAL_SPI_TransmitReceive() by placing timestamps before and after the function call, using the DWT cycle counter (DWT->CYCCNT) available on the Cortex-M3.
Here is the code used for testing, the tx and rx buffer are globally defined of size 5000 and datatype uint8_t:
/* Enable trace and debug block */
CoreDebug->DEMCR |= CoreDebug_DEMCR_TRCENA_Msk;
/* Reset the cycle counter */
DWT->CYCCNT = 0;
/* Enable the cycle counter */
DWT->CTRL |= DWT_CTRL_CYCCNTENA_Msk;
uint32_t previous_count=0;
uint32_t diff=0;
tx_buffer[0] = status_reg_read_opcode;
// starting to receive status byte continuously
HAL_GPIO_WritePin(GPIOB, GPIO_PIN_12, GPIO_PIN_RESET);
previous_count = DWT->CYCCNT;
HAL_SPI_TransmitReceive(&hspi2, tx_buffer, rx_buffer, 5000, 1000);
diff = DWT->CYCCNT - previous_count;
HAL_GPIO_WritePin(GPIOB, GPIO_PIN_12, GPIO_PIN_SET);
static void MX_SPI2_Init(void)
{
/* SPI2 parameter configuration*/
hspi2.Instance = SPI2;
hspi2.Init.Mode = SPI_MODE_MASTER;
hspi2.Init.Direction = SPI_DIRECTION_2LINES;
hspi2.Init.DataSize = SPI_DATASIZE_8BIT;
hspi2.Init.CLKPolarity = SPI_POLARITY_LOW;
hspi2.Init.CLKPhase = SPI_PHASE_1EDGE;
hspi2.Init.NSS = SPI_NSS_SOFT;
hspi2.Init.BaudRatePrescaler = SPI_BAUDRATEPRESCALER_4;
hspi2.Init.FirstBit = SPI_FIRSTBIT_MSB;
hspi2.Init.TIMode = SPI_TIMODE_DISABLE;
hspi2.Init.CRCCalculation = SPI_CRCCALCULATION_DISABLE;
hspi2.Init.CRCPolynomial = 10;
if (HAL_SPI_Init(&hspi2) != HAL_OK)
{
Error_Handler();
}
}
I have also attached my full main.c file.
Measured results
Below is the data I collected manually from the Expressions window in STM32CubeIDE (debug mode).
| No of bytes | cycles taken | actual time (us) | calculated datarate bytes/s | calculated time (us) | time difference | scaling factor (actual / cal) |
1000 | 270711 | 3759.8 | 1152000 | 888.8 | 2870.9 | 4.229 |
| 5000 | 1351484 | 18770.6 | 1152000 | 4444.4 | 14326.2 | 4.223 |
From this, it is clear that the actual transfer time is ~4.2× slower than the theoretical SPI transfer time.
Logic analyzer observations
I then captured the SPI signals using a logic analyzer (PulseView .sr file attached can be opened in pulseview software).
Key observations:
My current understanding / assumptions
In HAL_SPI_TransmitReceive(), the while loop:
while ((hspi->TxXferCount > 0U) || (hspi->RxXferCount > 0U))
{
/* Check TXE flag */
if ((__HAL_SPI_GET_FLAG(hspi, SPI_FLAG_TXE)) && (hspi->TxXferCount > 0U) && (txallowed == 1U))
{
*(__IO uint8_t *)&hspi->Instance->DR = *((const uint8_t *)hspi->pTxBuffPtr);
hspi->pTxBuffPtr++;
hspi->TxXferCount--;
/* Next Data is a reception (Rx). Tx not allowed */
txallowed = 0U;
}
/* Wait until RXNE flag is reset */
if ((__HAL_SPI_GET_FLAG(hspi, SPI_FLAG_RXNE)) && (hspi->RxXferCount > 0U))
{
(*(uint8_t *)hspi->pRxBuffPtr) = hspi->Instance->DR;
hspi->pRxBuffPtr++;
hspi->RxXferCount--;
/* Next Data is a Transmission (Tx). Tx is allowed */
txallowed = 1U;
}
if ((((HAL_GetTick() - tickstart) >= Timeout) && ((Timeout != HAL_MAX_DELAY))) || (Timeout == 0U))
{
hspi->State = HAL_SPI_STATE_READY;
__HAL_UNLOCK(hspi);
return HAL_TIMEOUT;
}
}
}These software checks introduce delay between successive writes to SPI->DR
This delay causes gaps in SCK, reducing effective throughput.
My questions
Motivation
I understand this might seem like going into excessive detail, but this is purely for learning purposes. I want to understand how SPI really works at the hardware level — not just from an API point of view, but the actual mechanics behind clock generation, data shifting, and timing.
Any insights, corrections, or references would be greatly appreciated.
Thank you for your time.
2026-01-14 2:33 AM - edited 2026-01-14 2:36 AM
Yes, this is a well-known "feature".
@Zaeem-Ahmed wrote:
- Why is the official STM32 HAL SPI API unable to keep the clock running continuously at the configured 9 MHz? otherwise why would it offer 9Mhz?
The HAL source is available for you to inspect.
You will see that HAL_SPI_TransmitReceive() does quite a lot of work between the end of one byte* and the start of the next.
You can improve matters by increasing the compiler optimisation level.
For maximum throughput, consider using DMA.
* Or whatever size transfer you are doing
@Zaeem-Ahmed wrote:2. Is SPI clock generation strictly tied to writes to SPI->DR?.
Yes.
This is fundamental to the operation of SPI; not specific to STM32: there is exactly one clock per bit transmitted.
If no bit is transmitted, there is no clock.
@Zaeem-Ahmed wrote:3. Is there any way (using HAL) to keep SCK running continuously while receiving data?
No - see above
@Zaeem-Ahmed wrote:4. Where can I study the internal hardware of the STM32F103 SPI peripheral in more detail like the complete logic diagram or gates circuit to check how the clock is controlled?
5. Where can I study the hardware of SPI peripheral of stm32f103rct6 in more details than ref manual, may be I can get a logic diagram or circuit diagram to see it in more detial specially how clock is being gating?.
The Reference Manual for the chip is the definitive document - ST (like other manufacturers) don't publish internal details.
You could try looking on the 'Documentation' tab of the Product Page to see if there are any useful Application Notes...
https://www.st.com/en/microcontrollers-microprocessors/stm32f103rc.html#documentation
@Zaeem-Ahmed wrote:6. What standard does the logic of SPI hardware follow? may be I can go through some SPI standards and understand this behaviour.
SPI is a long-established and widely-used standard - see, eg,
https://en.wikipedia.org/wiki/Serial_Peripheral_Interface
@Zaeem-Ahmed wrote:I am using SPI2 of STM32F103RCT6
Are you sure it's a genuine ST chip?
This part is widely cloned by 3rd parties, and sometimes clones are passed-off as ST originals
2026-01-14 3:33 AM
> 1. Is SPI clock generation strictly tied to writes to SPI->DR?
Yes. SCLK is directly tied to an ongoing transmission.
> 3. Is there any way (using HAL) to keep SCK running continuously while receiving data?
Find out what the HAL code does in between the transmissions.
As mentioned, the code is available for inspection.
I don't know what you exactly want to achieve in your application.
But check the SPI slave datasheet (AT45DB641), and see if you can organize read/write transfers in blocks, and initiate them with DMA.
Most memory device slaves have some "read block" command, were the master only transmits the start address, and the slave returns values from incremental addresses in following reads, until /SS is deasserted.