2018-08-23 10:32 PM
Hi,
i am trying to use I2C1 as a slave with interrupt
But after initializing the I2C
i am calling the following to set it to slave and receiver over interrupt
if(HAL_I2C_Slave_Receive_IT(&I2cHandle, (uint8_t*)&bTransferRequest, 1)!= HAL_OK){
Error_Handler();
}
but all the time it fails to do so and enters the Error_Handler() bcoz the return value is HAL_Timeout
I know about the Errata is mentioned regarding this issus
Can anyone provide a sample source for this ?
Thanks,
-Aditya
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.