2017-03-20 8:48 PM
Hi,
I am doing a work with stm32f103 adc.The adc is triggered by tim8,and it works,but it cause a triangular wave on input.
what's wrong ?
The input pin is PA1,code is as below:
/* ADC1 init function */
void MX_ADC1_Init(void){ADC_ChannelConfTypeDef sConfig;
/**Common config
*/ hadc1.Instance = ADC1; hadc1.Init.ScanConvMode = ADC_SCAN_DISABLE; hadc1.Init.ContinuousConvMode = DISABLE; hadc1.Init.DiscontinuousConvMode = DISABLE; hadc1.Init.ExternalTrigConv = ADC_EXTERNALTRIGCONV_T8_TRGO; hadc1.Init.DataAlign = ADC_DATAALIGN_RIGHT; hadc1.Init.NbrOfConversion = 1;HAL_ADC_Init(&hadc1);
/**Enable or disable the remapping of ADC1_ETRGREG:
* ADC1 External Event regular conversion is connected to TIM8 TRG0 */ __HAL_AFIO_REMAP_ADC1_ETRGREG_ENABLE();/**Configure Regular Channel
*/ sConfig.Channel = ADC_CHANNEL_1; sConfig.Rank = 1; sConfig.SamplingTime = ADC_SAMPLETIME_1CYCLE_5; HAL_ADC_ConfigChannel(&hadc1, &sConfig);}
void MX_TIM8_Init(void)
{TIM_ClockConfigTypeDef sClockSourceConfig;
// TIM_SlaveConfigTypeDef sSlaveConfig; TIM_MasterConfigTypeDef sMasterConfig;htim8.Instance = TIM8;
htim8.Init.Prescaler = 20; htim8.Init.CounterMode = TIM_COUNTERMODE_UP; htim8.Init.Period = 140; htim8.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1; htim8.Init.RepetitionCounter = 0; HAL_TIM_Base_Init(&htim8);sClockSourceConfig.ClockSource = TIM_CLOCKSOURCE_INTERNAL;
HAL_TIM_ConfigClockSource(&htim8, &sClockSourceConfig);/* sSlaveConfig.SlaveMode = TIM_SLAVEMODE_DISABLE; sSlaveConfig.InputTrigger = TIM_TS_ITR0; HAL_TIM_SlaveConfigSynchronization(&htim8, &sSlaveConfig);*/ sMasterConfig.MasterOutputTrigger = TIM_TRGO_UPDATE; sMasterConfig.MasterSlaveMode = TIM_MASTERSLAVEMODE_ENABLE; HAL_TIMEx_MasterConfigSynchronization(&htim8, &sMasterConfig);}
main()
{
.......
MX_ADC1_Init();
MX_TIM8_Init();
HAL_ADC_Start_IT(&hadc1);
HAL_TIM_Base_Start(&htim8);......
}