cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F0xx ADC Interrupt will not fire

mcgilvra2
Associate II
Posted on October 16, 2015 at 23:07

Using the STM32F072. Have set up the ADC to fire interrupt on end of conversion. It is not firing. I generated code using the latest STM32-CubeMX tool. Attached are resultant adc.c and adc.h. Also attached is full main. Below is pertinent part of main. I set a break-point in ADC1_COMP_IRQHandler() in interrupts.c (also attached) and it never fires. To verify that any interrupts were working I also set a breakpoint at SysTick_Handler() in interrupts.c and it fires fine. Any help would be greatly appreciated.

int main(void)

{

  hal_init();

  sysclock_init();

  gpio_init();

  //adc_init();

  MX_ADC_Init(); //McG

  MX_TIM2_Init(); //mcg

  __GPIOA_CLK_ENABLE(); //mcg This seems to be missing, can't find it anywhere so we'll do it here. stm32f0xx_hal_adc.c say's we have to.

  __GPIOB_CLK_ENABLE(); //mcg Ditto

  HAL_ADC_Start_IT(&hadc); //mcg start ADC in interrupt mode.

  spi_init();

  vhf_init();

  uhf_init();

  sensors_init();

  rs485_init();

  gps_init();

  ir_efs_init();

  // After delay, shut off WS circuit

  HAL_Delay(100);

  uint8_t wet_wakeup = HAL_GPIO_ReadPin(WATERSENSE);

  HAL_GPIO_WritePin(WATERSENSE_ENABLE, GPIO_PIN_SET);

  if(wet_wakeup)

 rs485_wakeup(); // Wake up lower units

  // Start watchdog

  watchdog_init();

  // Software timers

  uint32_t last_sensors = HAL_GetTick();

  uint32_t last_led = HAL_GetTick();

  uint32_t last_wakeup = HAL_GetTick();

  uint32_t last_engineering = HAL_GetTick();

  uint32_t last_rs485_process = HAL_GetTick();

  while (1)

  {.......

#stm32-stm32f0-adc
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0