2015-11-12 12:06 AM
Hi,
I am using STM32F072C8 uC and i configrated USART1 as 9600 bps. When I was sending some data,i don't receive correctly any data(when my serial port program set 9600bps).But i change my program baudrate as 14400bps and its work. My code ;USART_InitTypeDef USART_InitStructure;
GPIO_InitTypeDef GPIO_InitStructure;
SystemCoreClockUpdate();
// ***
SysTick_Config(SystemCoreClock / 1000);
// ***
syscore=SystemCoreClock;
RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOA, ENABLE);
RCC_APB2PeriphClockCmd(RCC_APB2Periph_USART1,ENABLE);
GPIO_PinAFConfig(GPIOA, GPIO_PinSource9, GPIO_AF_1);
GPIO_PinAFConfig(GPIOA, GPIO_PinSource10, GPIO_AF_1);
/* Configure USART1 pins: Rx and Tx ----------------------------*/
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_9 | GPIO_Pin_10;
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;
GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;
GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_UP;
GPIO_Init(GPIOA, &GPIO_InitStructure);
USART_InitStructure.USART_BaudRate = 9600;
USART_InitStructure.USART_WordLength = USART_WordLength_8b;
USART_InitStructure.USART_StopBits = USART_StopBits_1;
USART_InitStructure.USART_Parity = USART_Parity_No;
USART_InitStructure.USART_HardwareFlowControl = USART_HardwareFlowControl_None;
USART_InitStructure.USART_Mode = USART_Mode_Rx | USART_Mode_Tx;
USART_Init(USART1, &USART_InitStructure);
USART_Cmd(USART1,ENABLE);
2015-11-12 2:25 AM
I fixed this fault.I was change HSE value as 12MHz and works now.
2015-11-12 2:40 AM
Hi tunder.pinyin,
Thank you for posting your findings and how you fixed the issue, it is good to hear that it was solved. -Syrine-