cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F051K8T6 IC doesn't show the diode value across the Vdd and Vss pins. It shows OL in the multimeter display.

AKuma.22
Associate
 
This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Peter BENSCH
ST Employee

There is no diode across VDD and VSS, but there are so called parasitic diodes at the GPIOs. But these parasitic diodes arise as a by-product during production of the die and must not be used as a diode.

Please explain your expectations, maybe we can sort that out.

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
TDK
Super User

FWIW, on my STM32F4 disco board, my multimeter shows 0.378V when connected between GND and VDD. I assume it's grabbing the voltage protection diode voltage.

I agree it's an odd measurement to make.

If you feel a post has answered your question, please click "Accept as Solution".