cancel
Showing results for 
Search instead for 
Did you mean: 

STM32f042 CAN attempt

fred bar
Senior
Posted on August 15, 2017 at 19:55

Hello.

I am using a stm32F042 for some CAN communications, alongside a SN65HVD230 as transceiver.

I have two boards (my own) using both those ICs.

I made a simple program, based on the STM32 example, from a STMCube initial code.

Actually, i have problems making my two modules discussing. Sending � works � (in the way that the can outputs things), but receiving does not.

I�ll go into code later eventually, but i first have a question about what the STM32F outputs. Please see the CAN oscilloscope trace below. CAN_L and CAN_H signals are cyan and yellow, blue is what comes out of the transceiver on receiving side.

This signal is generated, then the sender enters timeout. It seems there are a dozen attempts, then a burst of much shorter pikes. 

What bothers me is that i cannot relate this signal to anything i could gather from docs, like the CAN frame description..

https://upload.wikimedia.org/wikipedia/commons/5/5e/CAN-Bus-frame_in_base_format_without_stuffbits.svg

At the moment, i do believe the receiver does not understand the data that is sent, as it looks like garbage to me.

Any idea, please?

#problem #can
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0