2017-09-28 8:58 AM
Hi all,
I'm trying to send an HTTP message through Ethernet interface using a WIFI external device. For this, I use HAL_UART functions as shown:
HAL_UART_Transmit(huart, messageTX,lengthOfmessage, timeoutTX);
UART has the following configuration:
static void MX_USART1_UART_Init(void)
{
huart1.Instance = USART1;
huart1.Init.BaudRate = 115200;
huart1.Init.WordLength = UART_WORDLENGTH_8B;
huart1.Init.StopBits = UART_STOPBITS_1;
huart1.Init.Parity = UART_PARITY_NONE;
huart1.Init.Mode = UART_MODE_TX_RX;
huart1.Init.HwFlowCtl = UART_HWCONTROL_NONE;
huart1.Init.OverSampling = UART_OVERSAMPLING_16;
huart1.Init.OneBitSampling = UART_ONE_BIT_SAMPLE_DISABLE;
huart1.AdvancedInit.AdvFeatureInit = UART_ADVFEATURE_NO_INIT;
if (HAL_UART_Init(&huart1) != HAL_OK)
{
_Error_Handler(__FILE__, __LINE__);
}
}
My tests results was (monitoring with Wireshark software):
1) Set the parameters as follows:
- messageTX = 'GET /registro/index.php/?solicitud=Hello HTTP/1.1\ \r\n Host:192.168.1.116\r\n\r\n'
- lengthOfmessage = 75
- timeoutTX = 100
Results are OK, messageTX is successfully sent
2) Set the parameters as follows:
- messageTX = GET /registro/index.php/?solicitud=<horfeus><firma><IP>192.168.1.160</IP><TipoCliente>4</TipoCliente><tiempo>23/01/2017-04:57:04</tiempo><edificio>53</edificio><TipoAula>6</TipoAula><aula>MA21FPLA1</aula><serie>00352738</serie></firma></horfeus> <horfeus><firma><IP>192.168.1.160</IP><TipoCliente>4</TipoCliente><tiempo>23/01/2017-04:57:04</tiempo><edificio>53</edificio><TipoAula>6</TipoAula><aula>MA21FPLA1</aula><serie>00352738</serie></firma></horfeus> HTTP/1.1\ \r\n Host:192.168.1.116\r\n\r\n'
- lengthOfmessage = 275
- timeoutTX = 100
Here, results are NOK, messageTX is not successfully sent. In Wireshark SW I receive a message with size 19 bytes. I think this size 19 indicates the size that exceeds my messageTX, i.e.:
messageTX(275 bytes) - messageReceived(19 bytes) = 256 bytes
So, it's possible that STM32f030 UART interface limits my messageTX size in 256 bytes?
Please, help me.
Thanks in advance.
Solved! Go to Solution.
2017-09-28 9:22 AM
Hello!
through Ethernet interface using a WIFI external device.
UART is capable to send more than 256 Bytes by calling HAL_UART_Transmit(UART_HandleTypeDef *huart, uint8_t *pData, uint16_t Size, uint32_t Timeout). (Also IT Versions)
Is WiFi external device capable to handle more than 256 Bytes?
Check also the definition of 'message_length' in your code if it has 8bit width.
Regards
vf
2017-09-28 9:22 AM
Hello!
through Ethernet interface using a WIFI external device.
UART is capable to send more than 256 Bytes by calling HAL_UART_Transmit(UART_HandleTypeDef *huart, uint8_t *pData, uint16_t Size, uint32_t Timeout). (Also IT Versions)
Is WiFi external device capable to handle more than 256 Bytes?
Check also the definition of 'message_length' in your code if it has 8bit width.
Regards
vf
2017-09-28 9:22 AM
>>So, it's possible that STM32f030 UART interface limits my message TX size in 256 bytes?
It is improbable, the USART one has a single byte holding register. Transmission would be limited by the data you provide, and the realistic transmission time for that data vs timeout.
Does your device require flow control?
2017-10-02 12:16 PM
Yes! Problem was in lengthOfmessage definition (uint8_t in my case).
Thanks for your suppor! =)