Skip to main content
tomaz
Visitor II
April 28, 2015
Question

STM32F030 input protection diodes

  • April 28, 2015
  • 1 reply
  • 669 views
Posted on April 28, 2015 at 13:29

Hello!

I've been reading through the reference manual of the F030 and noticed the structure of the GPIOs ... I've noticed they don't have any input protection diodes. The F100 and others have two clamping diodes on 3.3V and 5V tolerant pins. Do they really have no protection? How to they survive ESD events?

thanks
    This topic has been closed for replies.

    1 reply

    Tesla DeLorean
    Guru
    April 28, 2015
    Posted on April 28, 2015 at 16:25

    I'd suspect the diagram has just be over simplified for the target audience, they are still there. If you hit any of the parts with sufficient energy the silicon is going to evaporate, if you need stronger protection you'd want to add it externally. Things that people touch like USB connectors, or SD Card sockets, being specific areas of concern.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..