2013-09-23 5:34 AM
Hello!
I want to get defined number of samples at constant sample rate. I used ADC1 triggered by TIM15 TRGO signal and DMA in normal (not circular) mode with interrupt on transfer complete. Something is wrong, DMAinterrupt is not
generated
. When I remove DMA configuration and configure ADC interrupt on conversion complete - it works, and sampling frequency is OK. uC: STM32F051R8T6 Code:#define SAMPLING_FREQUENCY 1000
#define LEN 128
#define ADC1_DR_Address 0x40012440
volatile uint16_t ADC_value;
volatile uint16_t ADC_tbl[LEN];
volatile uint16_t idx = 0;
void
ADCgo( void ){
ADC_InitTypeDef ADC_InitStructure;
GPIO_InitTypeDef GPIO_InitStructure;
TIM_TimeBaseInitTypeDef TIM_TimeBaseStructure;
DMA_InitTypeDef DMA_InitStructure;
NVIC_InitTypeDef NVIC_InitStructure;
/* DMA1 clock enable */
RCC_AHBPeriphClockCmd(RCC_AHBPeriph_DMA1 , ENABLE);
/* ADC1 Periph clock enable */
RCC_APB2PeriphClockCmd(RCC_APB2Periph_ADC1, ENABLE);
/* TIM15 Periph clock enable */
RCC_APB2PeriphClockCmd(RCC_APB2Periph_TIM15 , ENABLE);
/* GPIOC Periph clock enable */
RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOA, ENABLE);
/* Configure ADC Channel0 and 1 as analog input */
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_0 | GPIO_Pin_1;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AN;
GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL ;
GPIO_Init(GPIOA, &GPIO_InitStructure);
/* DMA1 Channel1 Config */
DMA_DeInit(DMA1_Channel1);
DMA_InitStructure.DMA_PeripheralBaseAddr = (uint32_t)ADC1_DR_Address;
DMA_InitStructure.DMA_MemoryBaseAddr = (uint32_t)ADC_tbl;
DMA_InitStructure.DMA_DIR = DMA_DIR_PeripheralSRC;
DMA_InitStructure.DMA_BufferSize = LEN;
DMA_InitStructure.DMA_PeripheralInc = DMA_PeripheralInc_Disable;
DMA_InitStructure.DMA_MemoryInc = DMA_MemoryInc_Enable;
DMA_InitStructure.DMA_PeripheralDataSize = DMA_PeripheralDataSize_HalfWord;
DMA_InitStructure.DMA_MemoryDataSize = DMA_MemoryDataSize_HalfWord;
DMA_InitStructure.DMA_Mode = DMA_Mode_Normal;
DMA_InitStructure.DMA_Priority = DMA_Priority_High;
DMA_InitStructure.DMA_M2M = DMA_M2M_Disable;
DMA_Init(DMA1_Channel1, &DMA_InitStructure);
/* DMA1 Channel1 enable */
DMA_Cmd(DMA1_Channel1, ENABLE);
/* Enable DMA1 Channel1 Transfer Complete interrupt */
DMA_ITConfig(DMA1_Channel1, DMA_IT_TC);
/* ADC DMA request in one shot mode */
ADC_DMARequestModeConfig(ADC1, ADC_DMAMode_OneShot);
/* Enable ADC_DMA */
ADC_DMACmd(ADC1, ENABLE);
/* ADCs DeInit */
ADC_DeInit(ADC1);
/* Initialize ADC structure */
ADC_StructInit(&ADC_InitStructure);
/* Configure the ADC1 in continous mode withe a resolutuion equal to 12 bits */
ADC_InitStructure.ADC_Resolution = ADC_Resolution_12b;
ADC_InitStructure.ADC_ContinuousConvMode = DISABLE;
ADC_InitStructure.ADC_ExternalTrigConvEdge = ADC_ExternalTrigConvEdge_Rising;
ADC_InitStructure.ADC_ExternalTrigConv = ADC_ExternalTrigConv_T15_TRGO;
ADC_InitStructure.ADC_DataAlign = ADC_DataAlign_Right;
ADC_InitStructure.ADC_ScanDirection = ADC_ScanDirection_Upward;
ADC_Init(ADC1, &ADC_InitStructure);
/* Convert the ADC1 Channel 0 with 5 Cycles as sampling time */
ADC_ChannelConfig(ADC1, ADC_Channel_0 , ADC_SampleTime_13_5Cycles);
// microphoneADC_DiscModeCmd(ADC1, DISABLE);
/* Set synchronous clock mode */
ADC_JitterCmd(ADC1, ADC_JitterOff_PCLKDiv2, ENABLE);
/* ADC Calibration */
ADC_GetCalibrationFactor(ADC1);
/* Enable ADCperipheral */
ADC_Cmd(ADC1, ENABLE);
/* Wait the ADCEN falg */
while
(!ADC_GetFlagStatus(ADC1, ADC_FLAG_ADEN));// TIMER 15:
TIM_DeInit(TIM15);
TIM_TimeBaseStructInit(&TIM_TimeBaseStructure);
/* Time base configuration */
TIM_TimeBaseStructure.TIM_Period = SystemCoreClock/SAMPLING_FREQUENCY - 1;
TIM_TimeBaseStructure.TIM_Prescaler = 0;
TIM_TimeBaseStructure.TIM_ClockDivision = TIM_CKD_DIV1;
TIM_TimeBaseStructure.TIM_CounterMode = TIM_CounterMode_Up;
TIM_TimeBaseInit(TIM15, &TIM_TimeBaseStructure);
/* TIM15 TRGO selection */
TIM_SelectOutputTrigger(TIM15, TIM_TRGOSource_Update);
/* TIM1 enable counter */
TIM_Cmd(TIM15, ENABLE);
/* Configure and enable DMA1 interrupt */
NVIC_InitStructure.NVIC_IRQChannel = DMA1_Channel1_IRQn;
NVIC_InitStructure.NVIC_IRQChannelPriority = 1;
NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE;
NVIC_Init(&NVIC_InitStructure);
/* ADC1 regular Software Start Conv */
ADC_StartOfConversion(ADC1);
}
void
DMA1_Channel1_IRQHandler( void ){
/* Test on DMA1 Channel1 Transfer Complete interrupt */
if
(DMA_GetITStatus(DMA1_IT_TC1)){
/* Clear DMA1 Channel1 Half Transfer, Transfer Complete and Global interrupt pending bits */
DMA_ClearITPendingBit(DMA1_IT_TC1);
}
printf_(
''*'' ); // BREAKPOINT}
#stm32f0-tim-adc-dma2013-09-23 6:12 AM
The problem has solved!
ADC_DeInit(ADC1) must be moved upper, before all ADC_xxx functions.