2015-10-05 11:52 PM
I have an STM32F0 which is receiving and transmitting serial data. When I send the data another board responds. If I poll RXNE looking for the data and store it in an array like this everything works:
//while ((USART1->ISR & USART_ISR_RXNE) == 0); //receiveArray[0] = USART1->RDR; //while ((USART1->ISR & USART_ISR_RXNE) == 0); //receiveArray[1] = USART1->RDR; //while ((USART1->ISR & USART_ISR_RXNE) == 0); //receiveArray[2] = USART1->RDR; //while ((USART1->ISR & USART_ISR_RXNE) == 0); //receiveArray[3] = USART1->RDR;However when I use the interrupt the first byte is received and then the interrupt continues to interrupt even after data is no longer being transmitted and the line is high. What makes it even stranger is that the RXNE bit is not even being set!The USART setup is below and then my interrupt function.void init_usart() { // clock to USART1 RCC->APB2ENR |= RCC_APB2ENR_USART1EN; // clock to GPIOA RCC->AHBENR |= RCC_AHBENR_GPIOAEN; // PA9 and PA10 to AF GPIOA->MODER |= GPIO_MODER_MODER9_1; GPIOA->MODER |= GPIO_MODER_MODER10_1; // remap to correct AF GPIOA->AFR[1] |= (1 << (1*4)); // remap pin 9 to AF1 GPIOA->AFR[1] |= (1 << (2*4)); // remap pin 10 to AF1 SystemCoreClockUpdate(); USART1->BRR = SystemCoreClock/9600; //0x1388; // enable with UE in CR1 //USART1->CR2 |= USART_CR2_SWAP; USART1->CR1 |= USART_CR1_UE; USART1->CR1 |= USART_CR1_RXNEIE; USART1->CR1 |= USART_CR1_RE; USART1->CR1 |= USART_CR1_TE;}void init_NVIC() { NVIC_EnableIRQ(USART1_IRQn);}void USART1_IRQHandler(void){ if ((USART1->ISR & USART_ISR_RXNE) == USART_ISR_RXNE){ receiveArray[(packetReceivedIndex)++] = (uint8_t)(USART1->RDR); }data =(uint8_t)(USART1->RDR); //dummy read just in case}2015-10-06 1:01 AM
And what is the content of USART1_ISR? Note, that overrun error is enabled through CR1.RXNEIE too.
JW2015-10-06 6:25 AM
I did include the interrupt for USART1. I tried to check the overflow and the framing error inside the interrupt like this:
// if (USART1->ISR & USART_ISR_ORE == USART_ISR_ORE){ // trace_puts(''overflow error''); // }but I never saw the overflow.v Is there something I am missing here?ThanksTracy2015-10-06 6:49 AM
Apologies there was a missing bracket - turns out I am getting overrun errors. But on the scope the data look perfect 1 stop bit high 1 start bit low. Why would this be causing an overrun. I am also doing nothing in the interrupt and nothing in the main code?
2015-10-06 6:59 AM
> I did include the interrupt for USART1. I tried to check the overflow and the framing error inside the interrupt
That seems OK. I don't see any other problem. But again, try to get somehow the value of USART_ISR register. That's what I'd do. I'd also double check (read out) the value of all control registers. In fact, I'd use a debugger to place a breakpoint inside the ISR and observe all the registers (bearing in mind that reading the data register clears the receive flag etc.) JW