2017-10-25 5:13 AM
Hi,
I try to implement I2C slave communication based on HAL Library (STM32F070) with another MCU. All functions that interest me include as argument
uint16_t Size parameter, for example:
HAL_StatusTypeDef HAL_I2C_Slave_Transmit_IT(I2C_HandleTypeDef *hi2c, uint8_t *pData, uint16_t Size);
HAL_StatusTypeDef HAL_I2C_Slave_Receive_IT(I2C_HandleTypeDef *hi2c, uint8_t *pData, uint16_t Size);
When I set the maximum buffer size in parameter uint16_t Size, the library stuck in:
/* All data are not transferred, so set error code accordingly */
if(hi2c->XferCount != 0U) { /* Set ErrorCode corresponding to a Non-Acknowledge */ hi2c->ErrorCode |= HAL_I2C_ERROR_AF; }So if I receive less data the HAL Library return HAL_I2C_ERROR_AF. It looks like the library functions work only for communication with fixed data frame lengths.
It is possible to use HAL libraries when data frame length may vary?
Thanks, Adrian