cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F0 eeprom emulation

DPark.2
Associate II

I implemented the eeprom function by referring to the link above. However, there is a phenomenon that the device restarts while switching pages(Looking at the internal code, there is a problem when deleting the page.).

Here's the part I modified.

1. Increased storage space due to large idle flash space.

2. Increased storage variables to 6.

3. If you keep saving only one of the saved variables, some variables will be lost when you switch pages, so all variables are saved together when saving.

//eeprom.h
 
//... 
 
#define VIRT_ADDR_VAR_A         0x00
#define VIRT_ADDR_VAR_B         0x01
#define VIRT_ADDR_VAR_C         0x02
#define VIRT_ADDR_VAR_D         0x03
#define VIRT_ADDR_VAR_E         0x04
#define VIRT_ADDR_VAR_F         0x05
 
//...
 
/* EEPROM start address in Flash */
#define EEPROM_START_ADDRESS  ((uint32_t)ADDR_FLASH_PAGE_90) /* EEPROM emulation start address */
 
/* Pages 0 and 1 base and end addresses */
#define PAGE0_BASE_ADDRESS    ((uint32_t)(EEPROM_START_ADDRESS))
#define PAGE0_END_ADDRESS     ((uint32_t)(ADDR_FLASH_PAGE_97 + (PAGE_SIZE - 1)))
 
#define PAGE1_BASE_ADDRESS    ((uint32_t)(ADDR_FLASH_PAGE_98))
#define PAGE1_END_ADDRESS     ((uint32_t)(ADDR_FLASH_PAGE_105 + (PAGE_SIZE - 1)))
 
//...
 
/* Used Flash pages for EEPROM emulation */
#define PAGE0                 ((uint16_t)0x0000)
#define PAGE1                 ((uint16_t)0x0008) /* Page nb between PAGE0_BASE_ADDRESS & PAGE1_BASE_ADDRESS*/
 
//...
 
/* Variables' number */
#define NB_OF_VAR             ((uint8_t)0x06)
 
//...

I even have example code, but I don't know what kind of stupid thing it is.

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
TDK
Super User

> #define PAGE1 ((uint16_t)0x0008)

I didn't dig into it, but looking at the comments suggests if PAGE0_BASE_ADDRESS is flash page 0 and PAGE1_BASE_ADDRESS is flash page 98, then PAGE0 should be 0, and PAGE1 should be 98.

Page 0 is usually used by your program and is not available to store data. Is that the case for you?

If you feel a post has answered your question, please click "Accept as Solution".

Thank you for your attention.

I modified the code in the question,

and fortunately PAGE0_BASE_ADDRESS is not PAGE 0.