cancel
Showing results for 
Search instead for 
Did you mean: 

stm32cubeprog

dgilioli9
Associate
Posted on May 18, 2018 at 16:09

Hello, in these days I'm using for the first time Stm32CubeProgrammer and I notice a little problem in version 1.0.0: In the page 'Erasing & Programming' the button 'Browse', used to select the directory where find the .Hex to use in order to program the device doesn't work. Is there any new Softeware version or way to solve the issue?

Thank you

Damiano
1 ACCEPTED SOLUTION

Accepted Solutions
Khouloud GARSI
Lead II
Posted on May 21, 2018 at 09:37

Hi

Gilioli.Damiano

‌,

This issue will be fixed in version 1.1.0

As a workaround ,please delete the following file:

c:\Users\%USERNAME%\STMicroelectronics\STM32CubeProgrammer\config.properties

Khouloud.

View solution in original post

3 REPLIES 3
Posted on May 18, 2018 at 16:30

Looks similar?

https://community.st.com/0D50X00009XkYp1SAF

Posted on May 18, 2018 at 17:36

Yes, but I'm able to perform the device program because I write (by hand...) the full path in the related window

Khouloud GARSI
Lead II
Posted on May 21, 2018 at 09:37

Hi

Gilioli.Damiano

‌,

This issue will be fixed in version 1.1.0

As a workaround ,please delete the following file:

c:\Users\%USERNAME%\STMicroelectronics\STM32CubeProgrammer\config.properties

Khouloud.