TCP Server and Client
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2018-05-20 11:58 PM
Posted on May 21, 2018 at 08:58
Hi
I'm using STM32F429ZI nucleo board and I'm trying this example to create a TCP Server:
#include 'mbed.h'
#include 'EthernetInterface.h' #include 'NetworkAPI/buffer.hpp'#include 'NetworkAPI/tcp/socket.hpp'using namespace network; #define PORT 1234#define MAX_PENDING 1EthernetInterface interface;
intmain(){ interface.init(); interface.connect(); printf('IP Address is %s\n\r', interface.getIPAddress()); tcp::Socket server; tcp::Socket client; Buffer buffer(256); if (server.open() < 0) { printf('Could not open server socket.\n\r'); return -1; } if (server.bind(PORT) < 0) { printf('Could not bind server socket to port '%d'.\n\r', PORT); return -1; } if (server.listen(MAX_PENDING) < 0) { printf('Could not put server socket into listening mode.\n\r'); return -1; } while (server.getStatus() == Socket::Listening) { if (server.accept(client) < 0) { printf('Warning: failed to accept connection.\n\r'); continue; } printf('Client connected '%s:%d'.\n\r', client.getRemoteEndpoint().getAddress().toString().c_str(), client.getRemoteEndpoint().getPort()); while (client.getStatus() == tcp::Socket::Connected) { buffer.flush(); switch (client.read(buffer)) { case -1: printf('Warning: failed to read data from client.\n\r'); break; case 0: printf('Connection closed.\n\r'); break; default: printf('Received %d bytes.\n\r%s\r', buffer.length(), (char *)buffer.data()); continue; } client.shutdown(); client.close(); } }}I have some issue with the EthernetInterface library. The error is in in the socket.h and endpoint.cpp.
How can I solve this problem?
Thank you
Nada
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0