cancel
Showing results for 
Search instead for 
Did you mean: 

STM32CubeMx STM32F3 CCM-RAM

Asantos
Senior
Posted on September 10, 2014 at 00:31

Hi,

  I would like to know if there are the option to create a IAR project in the STM32CubeMx that use CCM-RAM to run interrupt routines. If not. Are there plans to add it in the future?

Ari.
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
stm32cube-t
ST Employee
Posted on October 06, 2014 at 16:36

Hello,

STM32CubeMX does not support this specification configuration.

A manual update is required instead (refer to the application note:

http://www.st.com/web/en/resource/technical/document/application_note/DM00083249.pdf

).

 

We'll log your request as a possible enhancement for CubeMX.

Thank you.