cancel
Showing results for 
Search instead for 
Did you mean: 

STM32CubeMX project open bug : I can't open my project file since the last update.

Sebastien1
Associate II

Hello,

Since the last update of STM32CubeMX 4.26.1, I can't open my project file anymore.

Right after clicking on the 'open' button, the software freezes and one of the processor cores stays at 100%. The only available action, then, is to close the application.

As I can't download an older version of STM32CubeMX, I am out of options.

I attached the project file in question to this post.

Thanks in advance for your help.

This discussion is locked. Please start a new topic to ask your question.
10 REPLIES 10
Marco Stucchi
Associate

I have CubeMx version 5.2.1 and I cannot open an IOC project made with TouchGFX.

The error I get is :

2019-07-13 08:53:41,769 [INFO] ApiDbMcu:444 - Load IP Config File for GRAPHICS

Exception in thread "AWT-EventQueue-0" java.lang.ArrayIndexOutOfBoundsException: 8

     at com.st.microxplorer.plugins.projectmanager.gui.ProjectChoiceTab.updateToolChainSelection(ProjectChoiceTab.java:1895)