STM32CubeMX Multi-Drive Support with FatFS
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-05-16 1:46 AM
Hello,
I have STM32F7 discovery kit (Discovery kit with STM32F746NG MCU) . I have successfully tested microSDCard withKeil + STM32Cube able to Create/read/Write txt files.
I have also through UM1721 'Developing Applications on STM32Cube with FatFs'
STM32F746NG MCU has one only SDMMC interface .
So I have selected STM32F722VET6 (LQFP-100 Pins) with two SDMMC Interfaces.
My requirement is How I can access two microSDCard Simultaneously .
I want to copy the data from one SDCard to another SDCard ( or SPI Flash Memory or USB MSD).
1) How do I configure and access Multi-Drive Support with FatFS ( Different volume name or numbers) with STM32CubeMX ?
2) Can I configure and access FATFS with SPI Interface on any STM32 MCU with STM32Cube ?
Thanks in advance
KaranSolved! Go to Solution.
Accepted Solutions
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-05-18 6:59 AM
Hi
Singh.Gurpreet
,1) How do I configure and access Multi-Drive Support with FatFS (Differentvolume name or numbers)with STM32CubeMX?
Within CubeMX, toaccess to your two microSD Card simultaneously,you should first enable SDMMC1, SDMMC2 and FatFS. Then, on the generated code, you can handle both SD cards by indicatingthe drive numberin the path name. Here is an example hoping it helps you:
FIL f_src, f_dst;
f_open(&f_src, '0:srcfile.txt', FA_CREATE_ALWAYS |FA_READ);
f_open(&f_dst, '1:dstfile.txt', FA_CREATE_ALWAYS | FA_WRITE);
2) Can I configure and access FATFS with SPI Interface onany STM32 MCU with STM32Cube?
You can access to your SD card using SPI interface and enabling FatFs (user-defined within CubeMX). Unfortunately, most examples, that serve communication with SD card, use SDIO rather than SPI because of communication speed problem.
For more details about SPI & FATFS configuration to connect your SD card, Please refer to the following discussion
:https://community.st.com/thread/44247-cubemx-support-for-sdfatfsspi#comment-184565
It would be more efficient and functional to connect your SD card using SDIO, when it is allowed. You can refer to many examples in the firmware thathelp you:
\STM32Cube\Repository\STM32Cube_FW_F7_V1.0\Projects\STM32F722ZE-Nucleo\Applications\FatFS\FatFs_uSD
3) How function like(
/external-link.jspa?url=http%3A%2F%2Felm-chan.org%2Ffsw%2Fff%2Fdoc%2Fchdir.html
) is used to access Volume Name/No. ?The f_chdir function is used tochange the current working directoryof the current drive.
f_chdir('1:/dir1/dir2');
You can refer to this link to get more explication and details about this function
http://elm-chan.org/fsw/ff/doc/chdir.html
Best Regards,
Mohamed.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-05-16 4:40 AM
It might exceed the complexity of what CubeMX can achieve, you might need to construct the code manually by using the existing SDMMC examples and creating a second instance of the pin/peripheral configuration.
FatFs would need additional settings/options to create support for multiple drives/volumes, and you would need code to enumerate directories and copy between systems.
Up vote any posts that you find helpful, it shows what's working..
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-05-16 10:22 AM
Hello Clive One,
Thanks for update..
I am go through below thread .
https://community.st.com/0D50X00009XkXEPSA3
My current code for one SDMMC Mode is
/* Initialize all configured peripherals */
MX_GPIO_Init(); MX_SDMMC1_SD_Init(); MX_FATFS_Init();FATFS myFATFS;
FIL myFILE ; UINT testByte ;if(f_mount(&myFATFS,SD_Path, 0) == FR_OK)
{ char mypath[] = {'abc.txt\0'} ; f_open(&myFILE,mypath , FA_WRITE | FA_CREATE_ALWAYS) ; char mydata[] = {'Hello\0'} ; f_write(&myFILE, mydata , sizeof(mydata),&testByte ) ; f_close(&myFILE) ;}
But how and where I can drive number. ?
'You can pass the drive number in the path name or change the default drive with f_chdrive.'
--
Karan
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-05-17 12:11 AM
http://elm-chan.org/fsw/ff/doc/filename.html
'0:/driveone.txt'
'1:/drivetwo.txt'
Up vote any posts that you find helpful, it shows what's working..
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-05-17 9:56 PM
Thanks for Update Clive One..
Like below example ..
'0:/driveone.txt'
'1:/drivetwo.txt'
I have go thorough link provided by you ..
1) How function like((
http://elm-chan.org/fsw/ff/doc/chdir.html
) is used to access Volume Name/No. ?2) How Cube Generated code which understand to Read/Write from Volume Name/No.
Thanks..
Karan
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-05-18 6:59 AM
Hi
Singh.Gurpreet
,1) How do I configure and access Multi-Drive Support with FatFS (Differentvolume name or numbers)with STM32CubeMX?
Within CubeMX, toaccess to your two microSD Card simultaneously,you should first enable SDMMC1, SDMMC2 and FatFS. Then, on the generated code, you can handle both SD cards by indicatingthe drive numberin the path name. Here is an example hoping it helps you:
FIL f_src, f_dst;
f_open(&f_src, '0:srcfile.txt', FA_CREATE_ALWAYS |FA_READ);
f_open(&f_dst, '1:dstfile.txt', FA_CREATE_ALWAYS | FA_WRITE);
2) Can I configure and access FATFS with SPI Interface onany STM32 MCU with STM32Cube?
You can access to your SD card using SPI interface and enabling FatFs (user-defined within CubeMX). Unfortunately, most examples, that serve communication with SD card, use SDIO rather than SPI because of communication speed problem.
For more details about SPI & FATFS configuration to connect your SD card, Please refer to the following discussion
:https://community.st.com/thread/44247-cubemx-support-for-sdfatfsspi#comment-184565
It would be more efficient and functional to connect your SD card using SDIO, when it is allowed. You can refer to many examples in the firmware thathelp you:
\STM32Cube\Repository\STM32Cube_FW_F7_V1.0\Projects\STM32F722ZE-Nucleo\Applications\FatFS\FatFs_uSD
3) How function like(
/external-link.jspa?url=http%3A%2F%2Felm-chan.org%2Ffsw%2Fff%2Fdoc%2Fchdir.html
) is used to access Volume Name/No. ?The f_chdir function is used tochange the current working directoryof the current drive.
f_chdir('1:/dir1/dir2');
You can refer to this link to get more explication and details about this function
http://elm-chan.org/fsw/ff/doc/chdir.html
Best Regards,
Mohamed.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-05-20 6:09 AM
Hello,
Many of Thanks for update ...
I have ordered
http://www.st.com/en/evaluation-tools/nucleo-f722ze.html
. I will check you suggestion then updatewith in few days.
One more question If there direct function() in FATFS to
copy the files(txt, bmp more then 4MB)
from one SDCard to another SDCard.http://irtos.sourceforge.net/FAT32_ChaN/doc/en/open.html
Thanks again ..
--
Karan
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-05-20 8:16 AM
No, you'd need to enumerate through the directories, and copy the file data manually. This is more application level functionality, not file system level.
Basically using f_opendir(), f_readdir(), and then a copy function using f_open(), f_size(), f_read/write(), f_close(). You should probably allocate a large copy buffer to maximize transfer speed. Say 32KB, and then read/write buffer until all file content is processed. If you want attributes and time/date stamps to follow you'll need to manage that also.
Up vote any posts that you find helpful, it shows what's working..