2018-08-02 07:41 AM
Hi,
whenever I try to run the CubeMX updater on MacOS, using sudo, the update will fail with:
" Updater cannot write on Software Folder. It's probably due to a bad Acces Privilege."
I tried to give everyone, admin and me the right to read and write the folder and the app itself. No success!
Anybody knows how to make it work?
Thanks
2019-09-24 04:29 AM
Hey guys, I had the same problem but just now solved it. If anyone is still wondering how to solve this issue I did it the following way:
2020-02-04 11:12 PM
ALiss, thank you, This method worked for me. Cube 5.40 to 5.50 on macOS 10.15.3 Catalina.
2021-03-16 02:33 PM
I'm having this same problem now trying to update to 6.1.2 and from there to 6.2.0. I'm running Big Sur V 11.2.3.
I had this problem on one of my two Macs. On that Mac I had to use the sudo technique @ALiss mentioned above. THANK YOU, ALiss!
The other Mac installed normally without me having to invoke sudo.
2024-06-14 06:49 AM
Agree this works but really. MacOS support for CubeMX has been dreadful - having to extract the jar from previous versions, this installer is pretty shabby. It really grinds my gears when an alert has multiple spelling mistakes - this looks like some dodgy script kiddies work on Piratebay…