2018-11-12 12:01 AM
Nowadays nobody has single core CPU where project is building, so this option should be enabled by default, or configurable in CubeMX.
Solved! Go to Solution.
2019-04-26 12:11 AM
Looks like this "issue (not really an issue..)" is already solved in STM32CubeIDE, paraller build is on by default.
Thanks!
2019-01-02 11:05 AM
Any toughts?
2019-01-02 11:15 AM
Not exactly hard to click in Keil, or turning off browse information so it doesn't run like a compiler from 1985.
Personally use multi-core here so I can do OTHER things while the build occurs rather than saturate all of them.
2019-04-26 12:11 AM
Looks like this "issue (not really an issue..)" is already solved in STM32CubeIDE, paraller build is on by default.
Thanks!