cancel
Showing results for 
Search instead for 
Did you mean: 

STM32CubeMx ETH + FreeROTS

wangzhaofeng
Associate II
Posted on April 12, 2014 at 05:54

I have generated a project containing Ethernet and FreeROTS use STM32CubeMx tool on open407 or open429 but it does not work ;

In addition,i use STM32Cube_FW_F4_V1.1.0\Projects\STM324x9I_EVAL\Applications\LwIP\LwIP_HTTP_Server_Socket_RTOS on my STM324x9I_EVAL board it does not work as well

anybody can help?
This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Posted on April 12, 2014 at 14:18

Provide details of this Open429 board. (Website, pictures, schematic)

What causes Ethernet implementations not to work? Usually the PIN configurations, the configuration of the PHY, the mode/pins, and how and from where the clock(s) are sourced.

If the board has options/jumpers/solder-bridges make sure they are set correctly for ethernet connectivity.

Walk through the code, use a debugger, and try and refine the ''not work'' in to some identifiable reason.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
wangzhaofeng
Associate II