cancel
Showing results for 
Search instead for 
Did you mean: 

STM32CubeMX bug with STM32F030x (GPIO mode)

Andrey.St.
Associate II
Posted on April 03, 2014 at 18:16

After upgrading to version 4.1 .

There are the following problems .

When creating a new project (MCU STM32F030F4Px) and assigning output PA0 ( tab PINOUT) as GPIO_Input, then clicking in the tab Configuration -> GPIO everything right : GPIO mode: Input mode, it is possible to select the pull up / pull down.

But as soon as we add ( tab PINOUT) PA1 pin as an analog input , the tab Configuration -> GPIO changes occur PA0 pin changes the value on the GPIO mode GPIO_Mode_In and no ability to select pull up / pull down.

And bid.

In the generated file will be twice repeated line RCC_AHBPeriphClockCmd (RCC_AHBPeriph_GPIOA, ENABLE);Is it possible when generating code to check if previously set clock ports to avoid provoking the code redundancy .
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
stm32cube-t
Senior III
Posted on June 06, 2014 at 15:53

Hello,

Problem is fixed in MX 4.2.

Best regards.