cancel
Showing results for 
Search instead for 
Did you mean: 

STM32CubeMX Bug in Code Generation for NucleoF072

apperleye
Associate
Posted on December 15, 2015 at 19:10

There is a defect in the initialisation code that STM32CubeMZ generates for an STM32F072RB target if the high-speed external clock is selected. 

For some reason the code expects a value for constant 'HSI48_VALUE', even though the high-speed internal clock is not in use:

Drivers\CMSIS\Device\ST\STM32F0xx\Source\Templates\system_stm32f0xx.c

 

 

In function 'SystemCoreClockUpdate':

 

 Drivers\CMSIS\Device\ST\STM32F0xx\Source\Templates\system_stm32f0xx.c|287  

error: 'HSI48_VALUE' undeclared (first use in this function)

 

 

Drivers\CMSIS\Device\ST\STM32F0xx\Source\Templates\system_stm32f0xx.c|287

 

The workaround at this stage is to comment out the conditional code block in the file 'system_stm32f0xx.c' thus:

//&sharpif defined(STM32F042x6) || defined(STM32F048xx) || defined(STM32F072xB) || defined(STM32F078xx) || defined(STM32F091xC) || defined(STM32F098xx)

//      else if (pllsource == RCC_CFGR_PLLSRC_HSI48_PREDIV)

//      {

//        /* HSI48 used as PLL clock source : SystemCoreClock = HSI48/PREDIV * PLLMUL */

//        SystemCoreClock = (HSI48_VALUE/predivfactor) * pllmull;

//      }

//&sharpendif /* STM32F042x6 || STM32F048xx || STM32F072xB || STM32F078xx || STM32F091xC || STM32F098xx */

Eric

#!stm32-!cubemx-!stm32f072-!bug
This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Amel NASRI
ST Employee
Posted on December 17, 2015 at 14:29

Hi eapperley,

I cannot reproduce the reported issue selecting HSE as clock source for Nucleo_F072 board.

Could you please share your .ioc file?

-Mayla-

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

carmine
Associate II
Posted on December 17, 2015 at 16:35

I also confirm the issue, which is not properly a bug. It's caused by the fact that the

HSI48_VALUE

macro is defined inside the stm32f0xx_hal_conf.h, which is not included by the system_stm32f0xx.c.

However, the right workaround is to add stm32f0xx_hal_conf.h as include file using the GCC parameter -include (

-include''../include/stm32f0xx_hal_conf.h''

), and not decommenting that line of code.

Hope it helps.