cancel
Showing results for 
Search instead for 
Did you mean: 

STM32CubeMX 4.7.0 FreeRTOS osMessageCreate bug

lqdjdy
Associate
Posted on April 30, 2015 at 01:58

osMessageQId osMessageCreate (const osMessageQDef_t *queue_def, osThreadId thread_id)

{

  (void) thread_id;

  return xQueueCreate(queue_def->queue_sz, queue_def->item_sz);

  //return xQueueCreate(queue_def->queue_sz, (uint32_t) sizeof(queue_def->item_sz));   //-------------->Bug

}

if you want use a queue and the size larger than 4 bytes, osMessageCreate always give you a 4bytes queue. because sizeof(queue_def->item_sz) always return 4.

This discussion is locked. Please start a new topic to ask your question.
7 REPLIES 7
2dimka
Associate II
Posted on May 19, 2015 at 03:01

I have the same problem.

I try this:

return xQueueCreate(queue_def->queue_sz, queue_def->item_sz);

But osMessageGet() can return only (osEvent) type.

Therefore I was compelled to return to xQueueCreate() and other basic FreeRTOS calls.

james2399
Associate II
Posted on June 20, 2015 at 03:24

This bug is also present in STM32CubeMX 4.8.0 / STMCubeF4 1.6.0

So frustrating because the bugfix gets overwritten by CubeMX when you regenerate project code.

james2399
Associate II
Posted on July 17, 2015 at 05:00

Bug is still present in STM32CubeMX 4.9.0 / STM32CubeF4 1.7.0

Nesrine M_O
Lead II
Posted on July 23, 2015 at 15:24

Hi,

I will report the issue to our development team.

Thank you for the information and sorry for the inconvenience that it may bring.

-Syrine-

DD
Associate II
Posted on September 16, 2015 at 10:28

Hi, it seems that the bugfix on the STM32CubeF4 1.8.0 has highlighted another problem.

The functions osMessageGet and osMessageKeep will call the xQueueReceive(queue_id, &event.value.v, ticks) passing to it the address of the value.v element of a (osStatus) event variable; t

hen the &event.value.v is passed to the xQueueGenericReceive as the buffer (void * const pvBuffer) where to write the queue item you need to analyze.

Since the value.v is a single uint32_t, it is not correct to use it as a buffer where to store the queue item.

Moreover, if the queue item size is long enough, it will overwrite other stack elements and may lead the code to crash.

vapostolov
Associate
Posted on August 16, 2016 at 07:44

I hit the same issue. The problem is in the library template of the cmsis_os.h header file.

In my case I was running the current STM32CubeF4 release 1.13.0.

I worked around the issue by editing the template header file cmsis_os.h.

Change from:

const osMessageQDef_t os_messageQ_def_##name = \

 

{ (queue_sz), 

sizeof 

(type)  }

 

to:

const osMessageQDef_t os_messageQ_def_##name = \

 

{ (queue_sz), (type)  }

The location of the template header file cmsis_os.h on my computer is:

C:\Users\Vlad\STM32Cube\Repository\STM32Cube_FW_F4_V1.13.0\Drivers\CMSIS\RTOS\Template\cmsis_os.h

Posted on April 05, 2017 at 12:50

I confirm this in:

* @file cmsis_os.c

* @author MCD Application Team

* @date 22-January-2016

* @brief CMSIS-RTOS API implementation for FreeRTOS V8.2.3

looks like there should be a check on queue item size inside osMessageGet()

To avoid this bug is to not use queue with item size > 4 bytes