2011-09-29 4:30 AM
Hi,
I'm trying to use the USART from the STM32F103ZE to communicate with my Bluetoothmodul. In Adruino I use the USART like this:void setupBlueToothConnection()
{ blueToothSerial.begin(38400); delay(1000); sendBlueToothCommand(''\r\n+STWMOD=0\r\n''); sendBlueToothCommand(''\r\n+STNA=SeeduinoBluetooth\r\n''); sendBlueToothCommand(''\r\n+STAUTO=0\r\n''); sendBlueToothCommand(''\r\n+STOAUT=1\r\n''); sendBlueToothCommand(''\r\n +STPIN=0000\r\n''); delay(2000); // This delay is required. sendBlueToothCommand(''\r\n+INQ=1\r\n''); delay(2000); // This delay is required. } But how can I send this command's with the STM32 USART, I didnt found a solution? regards Alex #yet-another-example2011-09-29 6:24 AM
The forum, the FW library, and Keil/IAR, are replete with example code
.. USART_InitTypeDef USART_InitStructure; GPIO_InitTypeDef GPIO_InitStructure; RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOA, ENABLE); /* Enable GPIO A for USART2 Rx,Tx Pins */ RCC_APB1PeriphClockCmd(RCC_APB1Periph_USART2, ENABLE); /* Enable USART2 Clock */ /* Configure USART2 Tx (PA.02) as alternate function push-pull */ GPIO_InitStructure.GPIO_Pin = GPIO_Pin_2; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF_PP; GPIO_Init(GPIOA, &GPIO_InitStructure); /* Configure USART2 Rx (PA.03) as input floating */ GPIO_InitStructure.GPIO_Pin = GPIO_Pin_3; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_IN_FLOATING; GPIO_Init(GPIOA, &GPIO_InitStructure); USART_InitStructure.USART_BaudRate = 38400; USART_InitStructure.USART_WordLength = USART_WordLength_8b; USART_InitStructure.USART_StopBits = USART_StopBits_1; USART_InitStructure.USART_Parity = USART_Parity_No ; USART_InitStructure.USART_HardwareFlowControl = USART_HardwareFlowControl_None; USART_InitStructure.USART_Mode = USART_Mode_Rx | USART_Mode_Tx; USART_Init(USART2, &USART_InitStructure); USART_Cmd(USART2, ENABLE); /* Enable the USART */ .. See your other thread for string output code using the FW library void send_string(const char *s) { while(*s) { while(USART_GetFlagStatus(USART2, USART_FLAG_TXE) == RESET); USART_SendData(USART2, *s++); } }