cancel
Showing results for 
Search instead for 
Did you mean: 

STM32_USB-FS-Device_Lib Errors

Clifford1
Associate III
Posted on November 05, 2010 at 17:00

STM32_USB-FS-Device_Lib Errors

This discussion is locked. Please start a new topic to ask your question.
4 REPLIES 4
tsuneo
Senior
Posted on May 17, 2011 at 14:14

As Stefano pointed out on this topic, the delay routine touches SysTick timer in the STM32_USB-FS-Device_Lib for STM32F105-7. It causes unpredictable error on RTOS.

https://my.st.com/public/STe2ecommunities/mcu/Lists/ARM%20CortexM3%20STM32/ST%20USB_LIBS%203.2.0

Replace uDELAY(usec) and mDELAY(msec) with RTOS-specific delay routines.

These delay routines are #define'd on otgd_fs_cal.h

In the USB stack, both routines calls USB_OTG_BSP_uDelay() (hw_config.c), which touches to SysTick timer.

mDELAY(50 or 25) is used in these routines,

otgd_fs_cal.c: OTGD_FS_CoreInit(), OTGD_FS_SetDeviceMode()

otgd_fs_pcd.c: PCD_DevConnect(), PCD_DevDisconnect()

For Keil RL-RTX, os_dly_wait() fits to this purpose well.

uDELAY(5) is used in these routines,

otgd_fs_cal.c: twice in OTGD_FS_CoreReset(), OTGD_FS_FlushTxFifo(), OTGD_FS_FlushRxFifo()

uDELAY() is too short to replace with os_dly_wait(), which runs on system tick. You may need to write a custom routine, which polls STK_VAL of SysTick timer or other one.

Tsuneo

Clifford1
Associate III
Posted on May 17, 2011 at 14:14

Thanks Tsuneo, that seems to have resolved the issue.  Although some care is needed in the implementation since the delay can be called form an interrupt context.

The USB I/O now seems robust, however simply connecting the USB cable still affects the performance and functionality of other tasks in my application, so I shall need to investigate further.

Clifford1
Associate III
Posted on May 17, 2011 at 14:14

The remaining issues were in my code. All good now, thanks again.

tsuneo
Senior
Posted on May 17, 2011 at 14:14

> Although some care is needed in the implementation since the delay can be called form an interrupt context.

As of mDELAY(),

OTGD_FS_CoreInit(), OTGD_FS_SetDeviceMode(), PCD_DevConnect() and PCD_DevDisconnect() are called just from USB_Init() in this call tree.

USB_Init()

- pProperty->Init()

- - Virtual_Com_Port_init()

- - - USB_SIL_Init()

- - - - OTG_DEV_Init()

- - - - - PCD_Init()

- - - - - - OTGD_FS_CoreInit()

- - - - - - - OTGD_FS_SetDeviceMode()

- - - - - - - - mDELAY()

- - - PowerOn()

PowerOn()

PowerOff()

- USB_Cable_Config()

- - USB_DevConnect()

- - - PCD_DevConnect()

- - - - mDELAY()

- - USB_DevDisconnect()

- - - PCD_DevDisconnect()

- - - - mDELAY()

PowerOff() is not called from anywhere.

Usually, USB_Init() is included in the start-up task, invoked from os_sys_init().

Therefore(), we can replace mDELAY() with os_dly_wait() without any trouble.

As of uDELAY(), it is called from the IRQ Handler, too.

But no re-entrant occurs to uDELAY().

Therefore, simple timer-polling delay works well.

USB_Init()

- pProperty->Init()

- - Virtual_Com_Port_init()

- - - USB_SIL_Init()

- - - - OTG_DEV_Init()

- - - - - PCD_Init()

- - - - - - OTGD_FS_CoreInit()

- - - - - - - OTGD_FS_CoreReset()

- - - - - - - - uDELAY()

USB_Init()

- pProperty->Init()

- - Virtual_Com_Port_init()

- - - USB_SIL_Init()

- - - - OTG_DEV_Init()

- - - - - PCD_Init()

- - - - - - OTGD_FS_CoreInitDev()

- - - - - - - OTGD_FS_FlushTxFifo()

- - - - - - - - uDELAY()

- - - - - - - OTGD_FS_FlushRxFifo()

- - - - - - - - uDELAY()

OTG_FS_IRQHandler()

- STM32_PCD_OTG_ISR_Handler()

- - OTGD_FS_Handle_UsbReset_ISR()

- - - OTGD_FS_DEVICE_RESET

- - - - Device_Property.Reset()

- - - - - Virtual_Com_Port_Reset()

- - - - - - OTG_DEV_EP_Init()

- - - - - - - PCD_EP_Flush()

- - - - - - - - OTGD_FS_FlushTxFifo()

- - - - - - - - - uDELAY()

- - - - - - - - OTGD_FS_FlushRxFifo()

- - - - - - - - - uDELAY()

- - - OTGD_FS_FlushTxFifo()

- - - - uDELAY()

Tsuneo