cancel
Showing results for 
Search instead for 
Did you mean: 

STM32 USART Additional features?

JuM
Senior
Posted on June 26, 2018 at 08:17

Using STM32F0xx USART to communicate simplex in standard asynchronous mode (8 bits + parity) with many STM32F0xx slaves. Want to use additional USART features. Did understand and can use Idle and Break detection.

What about other USART features like Receiver Timeout, End-of-Block etc.

Sometimes RM091 clearly states that such a feature is available e.g. in LIN or Smartcard mode only, sometimes not.

Is there any clear doc about features which can be used in standard asynchronous USART mode?

Best regards Juergen.
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0