cancel
Showing results for 
Search instead for 
Did you mean: 

STM32 SPI DMA for External SPI DAC

fabio1
Associate II
Posted on January 25, 2014 at 21:34

Hi,

I am trying to sample some data using DMA and the internal ADC and send the same data , still using DMA to an external DAC using the SPI Internface, through an optoisolation barrier.

It all works great, I need 1MS/s  and this is not a problem.

Still I need to qualify the data using a NSS line and TI Mode works fine, but the lack of wait states makes my task hard.

The NSS is released on the 14th byte and re-issued on the 15th. Most of the DACs (I have been using DAC8311 for a while) need some time between the sync signal and the new data, so the NSS line needs to be inactive for a while between the subsequent data.

I could not find any suitable DAC.

Is the interface not suitable for such a task or am I missing something?

Thanks

Fabio

 

This discussion is locked. Please start a new topic to ask your question.
12 REPLIES 12
franck2
Associate II
Posted on November 24, 2014 at 15:46

Hi Fabio,

Same question as Blaz.

How did you configure the SPI? Do you require any additional code to start the transfer?

Thank you for your answers,

Franck

franck2
Associate II
Posted on November 24, 2014 at 15:48

Or did sending a word to the DMA controller may be sufficient to enable an SPI transaction?

franck2
Associate II
Posted on November 26, 2014 at 11:24

Hi Blaz,

I ask again my question:

How did you configure the SPI? Do you require any additional code to start the transfer?

Thanks for your reply.

Franck