cancel
Showing results for 
Search instead for 
Did you mean: 

STM32_PVD_need to set the reference Voltage

nanotronicsnss
Associate II

Hi i am using stm32H750VB as the IC for my project.I need to detect sudden power shutdown .I.e., i need to use PVD mode for detecting the sudden drop in voltage and save the EEPROM Contents.I need to use PVD using external analog voltage PIN RB7. But when i use this i cannot set the reference voltage (Cube MX) to my wish and the reference voltage is set around 1.20V (i think its a default value) and the corresponding interrupt function is generated(void HAL_PWR_PVDCallback ()). Kindly guide me through the steps for setting the reference voltage around 2.9V.

This discussion is locked. Please start a new topic to ask your question.
4 REPLIES 4
waclawek.jan
Super User

This is how PVD using PVD_IN pin works, read RM0433, Programmable voltage detector (PVD) chapter.

JW

nanotronicsnss
Associate II

Thanks for the reply...

I have read that and it is mentioned that "In this case PVD_IN voltage is compared to the internal VREFINT level" .

My question is how to change the value of "VREFINT".Is there a possibility of varying that voltage ?

waclawek.jan
Super User

> My question is how to change the value of "VREFINT".Is there a possibility of varying that voltage ?

No.

JW

nanotronicsnss
Associate II

ok ..thank u for your reply..