2012-03-21 4:56 AM
Hi,
I have to read a 15 bit parallel data coming from a camera sensor and one bit as a request signal which tells whether the micrcontroller should initiate memory transfer or not. Does FSMC has any trigger signal within itself so that I dont want to use any external interrupt or timer to trigger the transfer ? Please help me out.2012-03-27 6:47 PM
Timer can initiate the DMA transactions from GPIO to Memory.
In Source Peripheral address : Put GPIO DR In Destination : put RAM address..2012-03-29 1:37 AM
Hi Alokm
Thanks alot for confirming that !2012-03-29 6:46 AM
Hey!
I have a certain confusion regarding how does exactly the DMA transfer takes place from GPIO memory. How do I specify the address and tell the DMA that its a 15 bit parallel data which has to be tranferred at one got from GPIO to memory ?2012-03-29 7:02 AM
You're going to specify it as a 16-bit transfer (ie HalfWord), and point it at the GPIOx->IDR
Presuming you aligned your GPIO input bits sensibly, ie GPIOx.0-14 Now if it spans too many bits you might need to do it as 32-bit and extract the bits you want later.2012-04-05 6:22 AM
Is DMA transfer from GPIO pins to SRAM memory to memory transfer of data ?
2012-04-05 8:41 AM
Is DMA transfer from GPIO pins to SRAM memory to memory transfer of data ?
I'd kind of presume it could be a peripheral (non-increment) to memory (increment) transfer, but I haven't looked at all the busing/routing/muxing issues, and if you have a DMA controller on the right APB. My understanding is peripheral-to-memory can be done via a direct routing, where as memory-to-memory will require more cycles, and an intermediate buffer, to complete the transaction in at least two steps/phases. Either way, I don't suppose it would take more that 5-10 minutes to test/confirm what's workable, and what's not.2012-04-11 7:14 AM
Hi
I was trying to congifure the DMA to transfer from GPIOE IDR register to SRAM. The transfer should be initiated with an external trigger on TIM2_CH2 i.e. DMA1 Channel 3 STream 6. And here is what I wrote // Configure Channel 2 for external signal// TIM_ICInitStructure.TIM_Channel = TIM_Channel_2; TIM_ICInitStructure.TIM_ICPolarity = TIM_ICPolarity_Rising; TIM_ICInitStructure.TIM_ICSelection = TIM_ICSelection_DirectTI; TIM_ICInitStructure.TIM_ICPrescaler = TIM_ICPSC_DIV1; TIM_ICInitStructure.TIM_ICFilter = 0x0; //External clock mode 1 configured// TIM_ETRClockMode1Config(TIM2, TIM_ExtTRGPSC_OFF, TIM_ExtTRGPolarity_NonInverted, 0x00); TIM_SelectInputTrigger(TIM2, TIM_TS_TI2FP2); TIM_ICInit(TIM2, &TIM_ICInitStructure); /* TIM enable counter */ TIM_Cmd(TIM2, ENABLE); DMA_Cmd(DMA1_Stream6, ENABLE); TIM_DMACmd(TIM2,TIM_IT_Update,ENABLE); // Enable the Timer 2 Interrupt Request */ TIM_ITConfig(TIM2, TIM_IT_Trigger, ENABLE); while(1) { GPIO_ResetBits(GPIOD,GPIO_Pin_12|GPIO_Pin_14| GPIO_Pin_15); Delay(0xfffff); } DMA_config() { RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_DMA1,ENABLE); DMA_DeInit(DMA1_Stream7); DMA_InitStructure.DMA_Channel = DMA_Channel_3; DMA_InitStructure.DMA_PeripheralBaseAddr = GPIOE_IDR_Address ; DMA_InitStructure.DMA_Memory0BaseAddr = SRC_Buffer; DMA_InitStructure.DMA_DIR = DMA_DIR_PeripheralToMemory; DMA_InitStructure.DMA_BufferSize = 8; DMA_InitStructure.DMA_PeripheralInc = DMA_PeripheralInc_Disable; DMA_InitStructure.DMA_MemoryInc = DMA_MemoryInc_Enable; DMA_InitStructure.DMA_PeripheralDataSize = DMA_PeripheralDataSize_Byte; DMA_InitStructure.DMA_MemoryDataSize = DMA_MemoryDataSize_Byte; DMA_InitStructure.DMA_Mode = DMA_Mode_Circular; DMA_InitStructure.DMA_Priority = DMA_Priority_High; DMA_InitStructure.DMA_FIFOMode = DMA_FIFOMode_Disable; DMA_InitStructure.DMA_FIFOThreshold = DMA_FIFOThreshold_Full; DMA_Init(DMA1_Stream6, &DMA_InitStructure) } there is no DMA initiation whenever the external trigger happens !2012-04-11 7:15 AM
I even tried with TIM_DMA_Trigger instead of TIM_DMA_Update
2012-04-11 8:45 AM
TIM_DMACmd(TIM2,TIM_IT_Update,ENABLE); // ??
Surely that would be TIM_DMACmd(TIM2,TIM_DMA_Update,ENABLE); or more realistically TIM_DMACmd(TIM2,TIM_DMA_CC2,ENABLE); Since you want it to occur at the capture event, not when the timebase rolls-over, for which I don't see initialization code for. Or the pins or clocks. The secondary issue would be whether each pulse triggers a single transfer, or the entire block.2012-04-12 1:28 AM
I have to transfer a 15 bit data from GPIOE IDR to SRAM , only when there is an external trigger on TIM2 i.e. on PB3 pin. I have set the TIMER on Input capture mode. Moreover, an external trigger also initiates a DMA transfer on TIM2_CH2 DMA channel 3 stream 6. HEre is my compelte code :
/* =============================================================================== */ #ifdef __USE_CMSIS #include ''stm32f4xx.h'' #endif #define GPIOE_IDR_Address 0x40021000 #define GPIOE_ODR_Address 0x40021014 TIM_ICInitTypeDef TIM_ICInitStructure; DMA_InitTypeDef DMA_InitStructure; uint16_t SRC_Buffer[8] = {1,2,3,4,5,6,7,8}; void TIM_Config(void); void GPIO_Config(); void Delay(__IO uint32_t nTime); void TIM2_IRQHandler(void); int main(void) { GPIO_Config(); TIM_Config(); // Configure Channel 2 for external signal// TIM_ICInitStructure.TIM_Channel = TIM_Channel_2; TIM_ICInitStructure.TIM_ICPolarity = TIM_ICPolarity_Rising; TIM_ICInitStructure.TIM_ICSelection = TIM_ICSelection_DirectTI; TIM_ICInitStructure.TIM_ICPrescaler = TIM_ICPSC_DIV1; TIM_ICInitStructure.TIM_ICFilter = 0x0; TIM_ICInit(TIM2, &TIM_ICInitStructure); TIM_Cmd(TIM2, ENABLE); TIM_ITConfig(TIM2, TIM_IT_CC2, ENABLE); DMA_Cmd(DMA1_Stream6, ENABLE); TIM_DMACmd(TIM2,TIM_DMA_CC2,ENABLE); while(1) { GPIO_ResetBits(GPIOD,GPIO_Pin_12|GPIO_Pin_14| GPIO_Pin_15); Delay(0xfffff); } } void TIM_Config(void) { GPIO_InitTypeDef GPIO_InitStructure; NVIC_InitTypeDef NVIC_InitStructure; /* TIM2 clock enable */ RCC_APB1PeriphClockCmd(RCC_APB1Periph_TIM2, ENABLE); /* GPIOB clock enable */ RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOB, ENABLE); /* TIM2 channel 2 pin (PB.3) configuration */ GPIO_InitStructure.GPIO_Pin = GPIO_Pin_3; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_100MHz; GPIO_InitStructure.GPIO_OType = GPIO_OType_PP; GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL; GPIO_Init(GPIOA, &GPIO_InitStructure); /* Connect TIM pins to AF2 */ GPIO_PinAFConfig(GPIOB, GPIO_PinSource3, GPIO_AF_TIM2); /* Enable the TIM1 global Interrupt */ NVIC_InitStructure.NVIC_IRQChannel = TIM2_IRQn; NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 0; NVIC_InitStructure.NVIC_IRQChannelSubPriority = 0; NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE; NVIC_Init(&NVIC_InitStructure); RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_DMA1,ENABLE); DMA_DeInit(DMA1_Stream6); DMA_InitStructure.DMA_Channel = DMA_Channel_3; DMA_InitStructure.DMA_PeripheralBaseAddr = GPIOE_IDR_Address ; DMA_InitStructure.DMA_Memory0BaseAddr = SRC_Buffer; DMA_InitStructure.DMA_DIR = DMA_DIR_PeripheralToMemory; DMA_InitStructure.DMA_BufferSize = 8; DMA_InitStructure.DMA_PeripheralInc = DMA_PeripheralInc_Disable; DMA_InitStructure.DMA_MemoryInc = DMA_MemoryInc_Enable; DMA_InitStructure.DMA_PeripheralDataSize = DMA_PeripheralDataSize_Byte; DMA_InitStructure.DMA_MemoryDataSize = DMA_MemoryDataSize_Byte; DMA_InitStructure.DMA_Mode = DMA_Mode_Circular; DMA_InitStructure.DMA_Priority = DMA_Priority_High; DMA_InitStructure.DMA_FIFOMode = DMA_FIFOMode_Disable; DMA_InitStructure.DMA_FIFOThreshold = DMA_FIFOThreshold_Full; DMA_Init(DMA1_Stream6, &DMA_InitStructure); } void GPIO_Config() { GPIO_InitTypeDef GPIO_InitStructure; RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOD, ENABLE); /* Configure PD12, PD13, PD14 and PD15 in output pushpull mode */ GPIO_InitStructure.GPIO_Pin = GPIO_Pin_12 | GPIO_Pin_14| GPIO_Pin_15; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_OUT; GPIO_InitStructure.GPIO_OType = GPIO_OType_PP; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_25MHz; GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL; GPIO_Init(GPIOD, &GPIO_InitStructure); RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOE, ENABLE); GPIO_InitStructure.GPIO_Pin = GPIO_Pin_0|GPIO_Pin_1| GPIO_Pin_2| GPIO_Pin_3|GPIO_Pin_4| GPIO_Pin_5| GPIO_Pin_6|GPIO_Pin_7; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_IN; GPIO_InitStructure.GPIO_OType = GPIO_OType_PP; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_100MHz; GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL; GPIO_Init(GPIOE, &GPIO_InitStructure); } void TIM2_IRQHandler(void) { { GPIO_SetBits(GPIOD,GPIO_Pin_12|GPIO_Pin_14| GPIO_Pin_15); Delay(0xfffff); TIM_ClearFlag(TIM2, TIM_IT_CC2); } } void Delay(__IO uint32_t nTime) { while(nTime--) { } } The interrupt is working absolutely fine, but there is no DMA transfer !