2011-10-27 01:18 AM
Hi,
I configured STM32 I2C as slave. I have a master which read data of a valid STM32 I2C register address and then data of an STM32 I2C not valid register address, which is the data expected on the SDA line? After read access on the valid STM32 I2C register address, the STM32 I2C register address is automatically incremented as specified by the protocol? thanks brazov2011-10-27 06:44 AM
you do not asy if 1xx or 2xx
if 1xx have you read the errata? Erik