2018-04-05 9:09 AM
I want to send F0 slave address with 7 bit slave address mode by I2C.
When I try to send I got ADDR10 error. Because F0 is reserved 10 bit slave address sending value
please let me know there any way to send F0 for slave address with 7bit mode?
thanks
2018-04-05 1:21 PM
F0 is too large to fit in 7 bits,
which chip are to trying to work with ?
I will look it up.
2018-04-06 2:28 AM
hi,
I use STM32 NucleoF401RE development board and I want to write and read data to /from RT750
this chip has 7 bit slave address and 1 bit(first bit) read-write.
Also, this chip has 4 different register group and each register group has different slave address.
1.group register slave address is 1111000x, 2
.group register slave address is 1111010x,
3
.group register slave address is 1111100x and 4
.group register slave address is 1111110x,
x=read-write bit
if I want to write data to 3. and 4. group register with 7bit mode I can write. Because the slave addres is 11111000(0xF8),
11111100(0xFC) but if I want to write 1. and 2. register group with 7bit mode I cant write. because
the slave addres is
11110000(0xF0) and 11110100(0xF4), I have ADDR10 flag error and the comnunication is stoped.
when I use USB to I2C baord I can write and read data from RT750 by my computer.
2018-04-06 3:01 AM
I cannot find an RT750 do you have a link ?
2018-04-06 3:18 AM
this is speacial chip. you should sign NDA first. I can write and read data with EM78F641 (8 bit ELAN microcontroller)
by my assembler code. But STM32 is new for me I use first time. I use assembler to write code for microcontroller until now. It is first time I use STM32MX cupe and Keil with C. it is disaster for me. Actually I finished other part of software and they are ok. I have problem the smallest and last part of software it is I2C.
2018-04-07 2:08 PM
If you use HAL, look here
http://stm32f4-discovery.net/2015/07/hal-library-16-i2c-for-stm32fxxx-devices/
If you use SPL, look here
http://stm32f4-discovery.net/2014/05/library-09-i2c-for-stm32f4xx/