STM32 HardFault_Handle
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2014-08-07 7:13 AM
I have a problem in STMF103C8T7 and I can't find the solution.
The STM32 reads corrupt data in array and when reaching a certain memory adress it crashes.The array look like this:typedef struct{int32_t v1;int32_t v2;uint32_t v3;short v4;}V_Data;&sharpdefine DATA_LENGTH 850V_Data data[DATA_LENGTH];Reading index 670 to 696 results in corrupt data. When writing to index 697 HardFault Exception occures. Variables after the array can be read witthout problemsThe .map file looks like:0x20001268 other variable0x2000126c data array0x2000478c other variable, can be ead and written0x20004790 other variable, can be ead and written0x20004858 other variable, can be ead and written0x2000485c other variable, can be ead and writtenThe corrupt data starts at0x2000126c + 670 * 16 = 15436 => 0x20003C4CThe crash address is at0x2000126c + 697 * 16 = 15868 => 0x20003DFCThe STM32 has 20 kB SRAM and SRAM starts at adress 0x20000000 with size 0x00005000.I have put protection around pointeras and arrays which could access the data array.Since Hardfault exception occurs I suspects that there is something wrong in the memory mapping.Heap and stack are located on:.heap 0x20004a04 0x00x20004a04 __end__ = .0x20004a04 _end = __end__0x20004a04 end = __end__*(.heap*)0x20004a04 __HeapLimit = ..co_stack 0x20004a04 0x404 load address 0x0801377c0x20004a08 . = ALIGN (0x8)*fill* 0x20004a04 0x4 *(.co_stack .co_stack.*).co_stack 0x20004a08 0x400 ..\obj\startup_stm32f10x_md.o0x20004a08 pulStack0x20005000 __StackTop = (ORIGIN (ram) + 0x5000)0x20004bfc __StackLimit = (__StackTop - SIZEOF (.co_stack))0x20005000 PROVIDE (__stack, __StackTop)0x00000001 ASSERT ((__StackLimit >= __HeapLimit), region ram overflowed with stack)I am using GCC 4.8.2 and CooCox 1.7.6 #stm32- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2014-08-08 8:34 AM
''if i try to #include core_cmFunc.h
I get the following errors:'' Try including core_cm4.h or the one that is correct for your processor (I think core_cm4.h is for STM32F4 parts) It contains the #include for core_cmFunc.h plus the other includes it needs- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2014-08-08 9:40 AM
Thank again.
I have modifirying the Default handler to#include ''stackdebug.h''void Default_Reset_Handler(void){ /* Initialize data and bss */ unsigned long *pulSrc, *pulDest; /* Copy the data segment initializers from flash to SRAM */ pulSrc = &_sidata; for(pulDest = &_sdata; pulDest < &_edata; ) { *(pulDest++) = *(pulSrc++); } /* Zero fill the bss segment. This is done with inline assembly since this will clear the value of pulDest if it is not kept in a register. */ __asm('' ldr r0, =_sbss\n'' '' ldr r1, =_ebss\n'' '' mov r2, #0\n'' '' .thumb_func\n'' ''zero_loop:\n'' '' cmp r0, r1\n'' '' it lt\n'' '' strlt r2, [r0], #4\n'' '' blt zero_loop''); ClearStackArray(); SaveStack(); /* Setup the microcontroller system. */ SystemInit(); SaveStack(); /* Call the application's entry point.*/ main();}And when I print the stack array I getsp[0] = 20003F50sp[1] = 20003F50sp[2] = 20003EC8sp[3] = 20003EC8Thus the flash seems correct and the stack is wrong before even System_Init which brings mw to the question:could the copy from flash to ram mess up my stackpointer?pulSrc = &_sidata; for(pulDest = &_sdata; pulDest < &_edata; ) { *(pulDest++) = *(pulSrc++); } /* Zero fill the bss segment. This is done with inline assembly since this will clear the value of pulDest if it is not kept in a register. */ __asm('' ldr r0, =_sbss\n'' '' ldr r1, =_ebss\n'' '' mov r2, #0\n'' '' .thumb_func\n'' ''zero_loop:\n'' '' cmp r0, r1\n'' '' it lt\n'' '' strlt r2, [r0], #4\n'' '' blt zero_loop'');- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2014-08-08 9:46 AM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2014-08-08 9:55 AM
My mistake.
If I run without bootloader the stack pointer is correct- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2014-08-08 11:32 AM
Using an RTOS in the loader?
As I recall the alignment is actually 512 bytes, you could probably confirm by writing 0xFFFFFFFF to SCB->VTORUp vote any posts that you find helpful, it shows what's working..
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2014-08-09 5:19 AM
There is no RTOS in bootloader, it and all hardware functions are written by me.
Regarding the alignment it is aligned to 512 byte:0x3400/512 = 26I will test what value bootloader sets SP to and then what SP is when it is accessed in application. Feels like I am getting close...- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2014-08-11 3:23 AM
I finally found it.
Changed __set_MSP(*(uint32_t*) FLASH_START);to__set_MSP(*(uint32_t*) (FLASH_START));Which will result in:#define BL_FLASH_START 0x08000000#define BL_FLASH_SIZE 0x3400 // 13 kB#define FLASH_START (BL_FLASH_START + BL_FLASH_SIZE)__set_MSP(*(uint32_t*) 0x08000000 + 0x3400);__set_MSP(*(uint32_t*) (0x08000000 + 0x3400));Thus the MSP is set to valu at 0x08000000 and then add 0x3400, instead of reading data at address 0x08003400
- « Previous
-
- 1
- 2
- Next »