2008-10-22 12:04 AM
STM32 - Flash programming timeout
2011-05-17 3:48 AM
Hi,
I'm currently trying to program an STM32F103ZD with 284k Flash. In the beginning programming worked just fine but debugging was quiet slow. Thus, I checked the configurations and found out, that the controller has 284kB of flash memory but in the 'utilities' register the chip was set to 512kB and so I changed the settings of the memory address range to start at 0x08000000 with a size of 0x00047000. I tried to program, it seemed to work in the first place. Now, every time I try to program the device via JTAG interface it gives the error message ''flash timeout...'' or ''flash programming failed''. The full chip erase seems to work but nothing else. I tried the flash loader demonstrator but doesn't even get a connection. Is there any way I can revive the chip? Your help is much appreciated. Thanks. Steve [ This message was edited by: steve.haettasch on 22-10-2008 08:25 ]2011-05-17 3:48 AM
I just checked the eva-board again and recognized, that the controller on the board is not an STM32F103ZD, but an STM32F103ZE. Hence, the controller I tried to configure got completely wrong flash informations.
Is there any way to completely reset the chip to the factory settings?2011-05-17 3:48 AM
Apparently, the controller seems to have changed its mind and today it's programmable again
Problem solved. Thanks anyway.2011-05-17 3:48 AM
Hi Steve,
that's what I found so times. One day a feature works and the other it don't. The whole environment I'm working with (RIDE7/GNU) seems to be not very stable up to this time. Best regards Edi